[EVAL-ADV7613FEBZ] HDMI input and HDMI output

Hi,

The customer is trying to get EVAL-ADV7613FEBZ working using XRC.

He want to output the source image input via HDMI to HDMI and check it on the monitor.

In this case, should I execute "04-01 ADV7511 HDMI output" from the scripts in "ADV7613-VER.1.1c.txt"?

However, this script only sets the register of ADV7511, not the setting of ADV7613.

For example, is it correct to run the script "02-03 HDMI Input_LVDS Output Port A and B" and then run "04-01 ADV7511 HDMI output"?

Best regards.