Post Go back to editing

[ADV8005]Simultaneous output of SD encoder Y/C and RGB

Hi,

Currently, on my board, DAC1 to DAC6 of the ADV8005 are configured as follows.
I use only the SD encoder, not the ED/HD encoder.
DAC1: Y
DAC2: C
DAC3: Y
DAC4: C
DAC5: none
DAC6: none

I would like to change it as follows. Is it possible for the SD encoder output simultaneous Y/C and RGB?
If possible, please tell me which register should be set.
DAC1: Y
DAC2: C
DAC3: none
DAC4: G
DAC5: B
DAC6: R

Thank you.

Parents Reply
  • Hi,

      Yes,  ED/HD output standard support only the formats that are mentioned in the 0xE430 register.

      Note: ADV8005 includes a high-speed digital-to-analog video encoder. Its a 12-bit video DACs provide support for composite (CVBS), S-video (Y/C) and component (YPrPb/RGB) analog outputs in either SD, ED, or HD video formats video formats up to 1080p.

    Thanks,

    Poornima

Children
No Data