Post Go back to editing

looking for 10 bit parallel video data to MIPI CSI 2 converting SerDes IC

Thread Summary

The user is seeking a SerDes solution to convert 10-bit parallel video data with an 8 MHz PCLK to a MIPI CSI-2 interface. The ADV7482 is suggested, but it requires a minimum LLC clock frequency of 13.5 MHz, which may cause glitches with the 8 MHz PCLK. The support engineer will check for alternative components to meet the requirement.
AI Generated Content

Hi,

We are looking for SerDes Solution that converts 10 bit parallel video data with PCLK of 8MHz to MIPI CSI 2 interface. It means serializer with input of 10 bit parallel video data->long cable->Desrializer with MIPI CSI 2 output. If there is no SerDes solution, then direct converter IC is also acceptable. Any assistance is much appreciated.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.