Post Go back to editing

5V tolerant pins of ADV7611.

Hello,

I have a question about 5V tolerant pins of ADV7611.

Question :
 Do all of following pins support 5V tolerant?

 (A signal below 5.3V can input to these pins without power.)

 1pin HPA_A/INT2
 62pin DDCA_SCL
 63pin DDCA_SDA
 64pin RXA_5V

 Datasheet says:
  On Page 4,  The following pins are 5 V tolerant: DDCA_SCL, DDC_SDA, and RXA_5V.
  On Page 7,  The following inputs are 3.3 V inputs but are 5 V tolerant: DDCA_SCL and DDCA_SDA.
  On Page 8,  HPA_A/INT2 Miscellaneous digital A dual function pin that can be configured to output

                      a Hot Plug assert signal (for HDMI Port A) or an Interrupt 2 signal. This pin is 5 V tolerant.
  On Page 9,  62 DDCA_SCL HDMI input HDCP Slave Serial Clock Port A. DDCA_SCL is a 3.3 V input

                      that is 5 V tolerant.
                      63 DDCA_SDA HDMI input HDCP Slave Serial Data Port A. DDCA_SDA is a 3.3 V input

                      that is 5 V tolerant.

Thank you!
Best regards.

Parents
  • Hello,

    Thank you for your reply.

    About HPA_A/INT2,
    HPA_A/INT2 is open-drain pin.
    Reference Manual UG-180 says "A dual function open-drain pin that can be configured to
    output Hot Plug Assert signal (for HDMI Port A) or an Interrupt2 signal."
    So I think the "5V tolerant" means 5V pull-up can be connected to HPA_A/INT2 pin.

    Is "5V Tolerant Inputs to Gnd" applied to HPA_A/INT2 pin?
    Are the power supplies(DVD, DVDDIO, PVDD, TVDD and CVDD) required for external 5V pull-up?

    Thank you!
    Best regards.

Reply
  • Hello,

    Thank you for your reply.

    About HPA_A/INT2,
    HPA_A/INT2 is open-drain pin.
    Reference Manual UG-180 says "A dual function open-drain pin that can be configured to
    output Hot Plug Assert signal (for HDMI Port A) or an Interrupt2 signal."
    So I think the "5V tolerant" means 5V pull-up can be connected to HPA_A/INT2 pin.

    Is "5V Tolerant Inputs to Gnd" applied to HPA_A/INT2 pin?
    Are the power supplies(DVD, DVDDIO, PVDD, TVDD and CVDD) required for external 5V pull-up?

    Thank you!
    Best regards.

Children
No Data