Hi,
I study ADI C2B interface and find that
- 8-/10-/12-bit interleaved Y/C data up to 148.5 MHz
Can ADV7992 / ADV7993 support YUV 4:2:2 ? or support YCbCr 4:2:2 only?
if not, what is difference between YUV and YCbCr for ADV799x ?
Thanks.
ADV7992
Recommended for New Designs
General
C2B transmits video and bidirectional control data over low cost, un-shielded differential pair cable
-40°C to +105°C temperature grade
32...
Datasheet
ADV7992 on Analog.com
ADV7993
Recommended for New Designs
General
2-wire serial microprocessor unit (MPU) interface (compatible with I2C) capable of operating in master or slave mode
-40°C to +105°C temperature...
Datasheet
ADV7993 on Analog.com
Hi,
I study ADI C2B interface and find that
Can ADV7992 / ADV7993 support YUV 4:2:2 ? or support YCbCr 4:2:2 only?
if not, what is difference between YUV and YCbCr for ADV799x ?
Thanks.
Hi,
YUV and YCbCr are used interchangeably. Sometimes signals in digital format are referenced as YUV but normally we refer to digital.
Please note that YCbCr used in digital video and sometimes called YUV (i.e Cb-U,Cr-V,Y-Y)
Thanks,
Poornima