Post Go back to editing

ADV7123 loopback with ADV7182

Hi,

We have a scenario mentioned below

  • ADV7393 loopback to ADV7182 with Monochrome PAL video
    • ADV7182 status register reads
      • 0x10: 0x48 and 0x13: 0x4C [Interlaced and 50Hz]
  • ADV7123 loopback to ADV7182 with Monochrome PAL video
    • ADV7182 status register reads
      • 0x10: 0xC9 and 0x13: 0x0D [50Hz], Interlaced not detected

HYSNC and VSYNC of ADV7393 are ANDed together and used as Composite Sync to ADV7123, whereas BLANK of ADV7123 is Data Enable kind of signal

Please let us now why Interlaced is not being detected during ADV7123 loopback

  • Hi,

    When referring the ADV7123 datasheet at Page17, It can support 60 Hz for a noninterlaced system, or 30 Hz for an interlaced system.

    Could you please try with 30Hz frame rate for interlaced input and let us know the result.

    Please note that ADV7123 is just a triple DAC with blanking added based on the control pins.  You control all timing so it can implement almost any analog format including the sync signals.  Interlaced formats is set by the input sync timing.

    Thanks,

    Poornima