Post Go back to editing

ADV3201 output termination

Thread Summary

The user is experiencing incorrect video signal levels at the load when using an ADV3201 with a 75 Ω load. The final answer suggests that the ADV3200/ADV3201 is optimized for 150 Ω differential loads, and proper termination of input and output signals is crucial for 75 Ω single-ended environments.
AI Generated Content

Good evening, we're using a ADV3201 with single ended supply (0-5V); the image attached is a schematic representation of our circuit. We use this to drive a video signal load (75 ohm). What we can monitor is that video signal level at the load is not correct (see point indicated). Can it be related to the resistor/Capacitor values we are using?

Parents Reply Children
No Data