trying to do HDMI output using ADV7535 and i.MX7D.

I am trying to do HDMI output using ADV7535 and i.MX7D.

I set the register of ADV7535 and was able to display the test pattern on the display in test mode, but the display from the CPU does not work.

I think that it is a problem of matching with the DSI output from the CPU, but please tell me about the case where HDMI output is performed with the following two settings according to ADV7535 Configuration Scripts.

1. 640 x 480p-60Hz DSI 24BPP --2 x DSI Lanes --RGB Out

2. 1024 x 768p-60Hz DSI 24BPP --2 x DSI Lanes --RGB Out

Could you give me some documentation on the DSI output signals (clock frequency, DSI signal content, etc.) for each setting?