Team,
We are currently facing a concern, the below s our configuration( please ignore the LVDS path)
We are getting an interlaced feed to the infotainment , which uses a ADV7281 decoder, when we read the status register 0x13 on 7281m we get a value of 0x69 confirming interlaced feed , also the register 0x45 on reading always returns 0xB6 which confirm even field , How do we ensure that the odd frames are received ? we want to try the deinterlacing on the SOC, but we are not sure if both the odd and even fields are making it to CSI peripheral, is there a setting or a way to ensure this?