Post Go back to editing

RSET of ADV7391

Thread Summary

The user inquires about configuring the ADA4431-1 in load drive mode with the AD7391, noting that the current range is insufficient for full-scale operation. The final answer suggests using the AD7391-ADA4433 schematic and hardware connection as a reference, and emphasizes the importance of the RSET resistor value for controlling full-scale output current. The AD7391 requires a 4.12 kΩ RSET resistor for low-drive mode (4.33 mA into a 300 Ω load).
AI Generated Content

The AD7391 can use load drive mode and the output current of 4.3mA is defined as full scale current operation at 300ohm load.
Now we are considering the configuration with ADA4431-1 in the load drive mode. The range is insufficient for full scale current operation, is there any table for the output voltage range by changing the value of Rset?

  • Hi,

     As per ADV739x specification, COMP and Rset pin definition as,

    RSET Controls the amplitudes of the DAC 1, DAC 2, and DAC 3 outputs.  For full-drive operation (for example, into a 37.5 Ω load), a 510 Ω resistor must be connected from RSET to AGND.
    For low-drive operation (for example, into a 300 Ω load), a 4.12 kΩ resistor must be connected from RSET to AGND.

    COMP Compensation Pin. Connect a 2.2 nF capacitor from COMP to VAA;

    ADV739x contains three DACs. All three DACs can be configured to operate in full-drive mode.Full-drive mode is defined as 34.7 mA full-scale current into a 37.5 Ω load, RL.Full drive is the recommended mode of operation for the DACs.

    Alternatively, all three DACs can be configured to operate in low-drive mode.
    Low-drive mode is defined as 4.33 mA full-scale current into a 300 Ω load, RL.

    The ADV739x contains an RSET pin. A resistor connected between the RSET pin and AGND is used to control the full-scale output current and, therefore, the output voltage levels of DAC 1, DAC 2, and DAC 3. For full-drive operation, RSET must have a value of 510 Ω and RL must have a value of 37.5 Ω. For low-drive opera-tion, RSET must have a value of 4.12 kΩ, and RL must have a value of 300 Ω. The resistor connected to the RSET pin should have a 1% tolerance.

    The ADV739x contains a compensation pin, COMP. A 2.2 nF compensation capacitor should be connected from the COMP pin to VAA.

    The ADA4433 application circuit should be from the CN0264 as below web link
    Circuit Note | CN0264 | A Robust Solution for Transmitting Composite Video with Output Short-to-Battery Protection | Ana…

    Thanks,

    Poornima

  • Thanks for the answer.
    I'd like to use the ADA4431, but does that mean I can't use the ADV739x combination to match the range, etc.?
    What is the background of your recommendation for ADA 4433?

  • Hi,

     ADV443x are same family, so we just we give an example for ADV7391-ADA4433 schematic and hardware connection.

     Also please refer expert suggestion when using ADV7391 with ADA4431 at https://ez.analog.com/video/f/q-a/100208/adv7391-cable-detection-not-working/297861#297861

    Thanks,

    Poornima