ADV7611 - 640x480p 30Hz and 600x600p @30Hz support

Hello,

I wanted a 640x480p @30Hz input video resolution for my application. I have the required video timing parameters and have generated the EDID for the same. When I probe the signals in FPGA using ILA I am observing that the video from the ADV7611 gives 1200+ data valid (data enable) for a single line. The expected data valid is 640 (as per standard video timing). I tried 640x480 @60Hz and it was giving proper data i.e. 640 valids per line. Hence am not sure if ADV7611 supports 640x480p @30Hz. Similar behavior is observed for 600x600 @30Hz. Could you let me know if 640x480p @30Hz and 600x600p @30Hz resolutions are supported by ADV7611. If yes can you share the register settings for the same.

Thank you,

Ronston

Parents
  • 0
    •  Analog Employees 
    on Aug 10, 2020 7:04 AM

    Hi,

    640x480p@30Hz,600x600@30Hz the pixel clock would be less than 25Mhz. In HDMI mode, video formats with TMDS rates below 25 M pixels/sec require pixel repetition in order to be transmitted over the TMDS link. When the ADV7611 receives this type of video format, it discards repeated pixel data automatically, based on the pixel repetition field available in the AVI InfoFrame. Please refer Page38 at ADV7611 Reference Manual (UG-180)

    HDMI requires a pixel clock above 20MHz.You need to turn on pixel repetition to get the TMDS clock to get the clock high enough to meet HDMI spec.

    Note: Pixel repetition is used to get the TMDS clock above the spec'd minimum of 20MHz.  When using pixel repetition the sink would need to ignore the duplicated pixels to get back down to a original format.  Note the AVI infoframe carries the pixel repetition information so the sink can respond correctly.

    Thanks,

    Poornima

  • Hello Poornima,

    Thank you for the reply.

    From the reply what I understood is that the ADV7611 does not support pixel frequency below 20MHz. Hence when any video with pixel clock below 20MHz is received it divides the clock until the frequency reaches above 20MHz and similarly repeats the input data twice (which is discarded by default). But as I was receiving 1280 valids (approx) instead of 640 can I assume that the repeated data is not being discarded? Will discarding it give me 640 valid data per line but at a clock of 26MHz instead?

    For clarification please consider the following case:

    For 640x480p @30Hz, the input pixel clock is 13MHz. Will the pixel repition done by ADV7611 convert this to 26MHz and then give this clock as output? Or will the clock frequency output from the ADV7611 remain 13MHz itself? And you could also tell me whether the data will remain on the line for 2clock cycles of the output clock ?

    Is there any script for configuring the ADV7611 to 640x480p @30Hz which will give me 13MHz clock and 640 valids? Do you know of any methods which can achieve this without any external help as it would be really helpful if I can generate it using ADV7611.

    Thank and Regards,

    Ronston

  • 0
    •  Analog Employees 
    on Aug 11, 2020 9:13 AM in reply to Ronston

    Hi,

      1. Will the pixel repetition done by ADV7611 convert this to 26MHz and then give this clock as output?

        No ADV7611 can't convert to 26Mhz, it can only discards the repeated pixel data automatically, based on the pixel repetition field available in the AVI InfoFrame, this could be done on source/Generator side. Or else you can't transmit over HDMI interface as per specification.

      2. Or will the clock frequency output from the ADV7611 remain 13MHz itself?

          Yes. Please let us know your Tx(Transmitter) chip.

     3. And you could also tell me whether the data will remain on the line for 2clock cycles of the output clock?

        Yes only when below 20MHZ, then the sink will drop extra pixel to get back to the correct pixel rate.

    Note: As per HDMI specification, HDMI cable require above 25MHZ pixel clock to be transmitted over the TMDS link.


    Thanks,

    Poornima

  • Hi Poornima,

    Thank you for the inputs.

    The video path is as follows:

    CPU --> ADV7611 --> FPGA --> ADV7511 --> Display.

    My register set configuration for the ADV7611 is as follows. It would be really helpful if you can suggest any changes needed to it for getting the actual video from the ADV7611 in the case where the clock is lower than 20MHz. I am able to get proper data using this configuration for remaining cases where my pixel clock is higher than 20MHz.

    {
    {0x98, 0x00, 0x05}, 
    {0x98, 0x01, 0x06}, 
    {0x98, 0x02, 0xF0},
    {0x98, 0x03, 0x40},
    {0x98, 0x04, 0xA2},
    {0x98, 0x05, 0x28},
    {0x98, 0x06, 0xA7},

    {0x98, 0x0B, 0x44},
    {0x98, 0x0C, 0x42},
    {0x98, 0x14, 0x7F},
    {0x98, 0x15, 0x80},
    {0x98, 0x19, 0x83},
    {0x98, 0x20, 0xF0},
    {0x98, 0x33, 0x40},

    {0x44, 0x6C, 0x00},
    {0x44, 0xBA, 0x01},

    {0x64, 0x40, 0x81},

    {0x68, 0x9B, 0x03},
    {0x68, 0x6F, 0x08},
    {0x68, 0x85, 0x1F},
    {0x68, 0x87, 0x70},
    {0x68, 0x57, 0xDA},
    {0x68, 0x58, 0x01},
    {0x68, 0x03, 0x98},
    {0x68, 0x4C, 0x44},
    {0x68, 0xC1, 0x01},
    {0x68, 0xC2, 0x01},
    {0x68, 0xC3, 0x01},
    {0x68, 0xC4, 0x01},
    {0x68, 0xC5, 0x01},
    {0x68, 0xC6, 0x01},
    {0x68, 0xC7, 0x01},
    {0x68, 0xC8, 0x01},
    {0x68, 0xC9, 0x01},
    {0x68, 0xCA, 0x01},
    {0x68, 0xCB, 0x01},
    {0x68, 0xCC, 0x01},
    {0x68, 0x00, 0x00},
    {0x68, 0x83, 0xFE},
    {0x68, 0x6F, 0x0C},
    {0x68, 0x85, 0x1F},
    {0x68, 0x87, 0x70},
    {0x68, 0x8D, 0x04},
    {0x68, 0x8E, 0x1E},
    {0x68, 0x1A, 0x8A},
    {0x68, 0x57, 0xDA},
    {0x68, 0x58, 0x01},
    {0x68, 0x6C, 0xA1}

    };

    Thanks and Regards,

    Ronston

  • 0
    •  Analog Employees 
    on Aug 12, 2020 11:07 AM in reply to Ronston

    Hi,

     Could you please configure the below register in ADV7511 as

        72 3b CA.

    Please note that in the manual pixel repeat selection case, the VIC sent in the AVI info frame will need to be set in register 0x3C so configure according to your resolution.

    The multiplication of the input clock must be programmed in 0x3B[6:5], and the pixel repeat value sent to the Rx must be programmed in 0x3B[4:3]. Refer section 4.3.4 at ADV7511W Programming Guide

    Also let us know the readback below register from ADV7611.

      68 05

    Thanks,

    Poornima

Reply
  • 0
    •  Analog Employees 
    on Aug 12, 2020 11:07 AM in reply to Ronston

    Hi,

     Could you please configure the below register in ADV7511 as

        72 3b CA.

    Please note that in the manual pixel repeat selection case, the VIC sent in the AVI info frame will need to be set in register 0x3C so configure according to your resolution.

    The multiplication of the input clock must be programmed in 0x3B[6:5], and the pixel repeat value sent to the Rx must be programmed in 0x3B[4:3]. Refer section 4.3.4 at ADV7511W Programming Guide

    Also let us know the readback below register from ADV7611.

      68 05

    Thanks,

    Poornima

Children
  • Hello,

    Sorry I was tied up with some other work.

    Currently I don't want to make any changes to ADV7511 register configuration. I am internally generating the video for the ADV7511 using XIlinx IP's.

    My concern is regarding ADV7611. I am not sure if it was a typo form your side for the following statement

    " Could you please configure the below register in ADV7511 (Did you mean ADV7611) as 72 3b CA."

    Awaiting your confirmation for the same.

    The readback from 68 05 register of ADV7611 should be done after the EDID configuration or before. Just wanted to confirm.

    Thanks and Regards,

    Ronston

  • 0
    •  Analog Employees 
    on Aug 17, 2020 9:13 AM in reply to Ronston

    Hi,

     That is not an typo, If you changed in ADV7511 Tx side, then the source will send the data according to that.

    The readback from 68 05 register of ADV7611 should be done after the EDID configuration or before. Just wanted to confirm.

       After EDID configuration.

    Thanks,

    Poornima

  • Hello,

    I did not update the ADV7511 register configuration. The reason for not updating is that my FPGA RTL code will throw an error if I dont receive the proper resolution and thus no data will be sent to ADV7511 unless I get the required resolution from ADV7611.

    The readback value from the 68 05 register of ADV7611 seems to be varying for different confiurations. I observed values 0x00 and 0xB0 when reading the said register. Will get back to you regarding the same after I confirm if the value is actually varying or not.

    What is the value that you are expecting from this particular read?

    Thanks and Regards,

    Ronston 

  • 0
    •  Analog Employees 
    on Aug 19, 2020 2:03 PM in reply to Ronston

     Hi,

       For all configuration it will remain 68 05[0:3] as "0000" i.e 1x.

       Unless u will change this value in 0x3B and 0x3C in ADV7511, 68 05 will not get updated for 640x480p@30Hz.

       Please note that 'Tooverride the VIC detection, the pixel repeat mode must be set to manual by setting register 0x3B[6:5] to 0b10 or 0b11. The desired VIC is input into 0x3C[5:0]'.

    Thanks,

    Poornima

  • Hi,

    I guess I was not able to explain my application to you clearly and thus there seems to be some misunderstanding.

    I connect my CPU to the ADV7611 through HDMI. The video coming from this is sent to the FPGA. Here packetization is done and sent out through transceiver and looped back. The received data is again sent to FPGA for depacketization.  The depacketized data is converted to video format using Xilinx IP's and then sent to the ADV7511 in YCbCr 422 format. This is then connected to a display using HDMI.

    The FPGA has overflow and underflow error detection. If the input video from the ADV7611 has more valids or less valids per line then these errors are indicated and no data will be sent to ADV7511. The issue here is only at the input side and not at the output. I dont want to add any additional logic in my FPGA code to remove the additional pixels coming from the ADV7611 for resolutions having pixel clock less than 20MHz. 

    So I am not clear as to why the ADV7511 configuration needs to be changed. Were you expecting that whatever data comes from ADV7611 will be sent to ADV7511 without any changes? Sorry but thats not the case here. Hence I dont think I can discard the repeated values at the ADV7511 cause this means I will have to configure my project for 1280x480 resolution instead of 640x480 so as to make sure the repeated values are also sent.

    My requirement is that I want 640 valids only from ADV7611 per line for 640x480p @30Hz resolution. I dont want to receive 1280 valids instead of 640 valids. So is it possible to do so by changing register configuration of ADV7611 only. I cant to do any make arounds with ADV7511 to discard these extra pixels cause it would not satisfy my project requirements. 

    In brief what I want to know is " Can I obtain only 640 valid pixels per line for 640x480p @30Hz resolution from the ADV7611 by changing any register configuration of only ADV7611?"

    Thanks and Regards,

    Ronston