Housing connector-(PWB pattern 50mm*)-FPC connector-(FPC pattern 70mm*)-FPC connector-(PWB pattern 50mm*)-Ain
* Both PWB pattern and FPC pattern have impedance matching at 75Ω.
Hi,
Legacy video uses 75 Ohm cables and traces. It only defines the Impedance, not a specific connector, so whatever pattern you need, you can use but its not dependent.
Please note that this all has to do with matching the impedance and keeping the amplitude correct. When using a 2x gain iso-amp with 75 Ohm series resistors, the 150 Ohm R1 is needed to get the amplitude correct. The impedance through the video paths must remain the same.
Thanks,
Poornima
As Poornima has said video is based on 75 Ohm impedance. If the cable from the housing to the board is kept at 75 Ohms you should be OK without differential op-amps. Differential op-amps are good for noisy environments. I am not sure what you mean by normal or solid pattern. If the cable from the housing to the PCB is 75 Ohms it's good
Often PCBs are designed for 50 Ohm traces so if the incoming video connector is 75 Ohms you can place the 24/51 Ohm resistors right next to the connector and convert the video path to 50 Ohms and run it to Ain. Also the 24/51 Ohm network is required to reduce the video amplitude to the working range of the ADV7280 input.
I you have mis-matches, you will see ghosting in the video depending on the length of the mismatch. Small segments of mismatch won't be a problem. Ghosting is caused by the distance a reflection has to travel and with a large pixel time width and signals speed of PCBs about 20 cm/ns, CVBS can handle some impedance mismatch lengths.
Hope this helps
I am very grateful for your helpful comments.
Thank you,
o-taka