Post Go back to editing

ADV7619: no audio from recent-vintage Mac mini

Thread Summary

The user is experiencing issues with the ADV7619 not receiving audio from a Mac mini, despite receiving an I2S clock and working with other sources. The CS_DATA_VALID bit is low, preventing audio sample rate detection. Clearing bits 2 and 3 of HDMI register 0x14 restores audio, but the function of these bits is unclear. The final answer suggests using the ADV7619 evaluation board to rule out custom hardware/software issues.
AI Generated Content

We are having a problem receiving audio from a recent Mac mini using the ADV7619.

We successfully receive audio for all other sources, and other sinks we've tried have no trouble with audio from the Mac.  In fact, if we run the video from the Mac into a splitter, our device gets no audio but the other sync gets it just fine.  We are supplying the EDID in this case, which advertises basic audio support only.

We *are* receiving an I2S clock consistent with 48 KHz, sampling rate, but no audio samples.

Here is a partial register dump when connected to the Mac (although it is not part of this dump I checked and confirmed that we are in HDMI mode, not DVI):

[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:893]:HDMI map 0x04 = 0x23
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:894]:  Audio PLL locked = 0x01
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:898]:IO map 0x7E = 0x1c
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:899]:  Audio FIFO Overflow raw = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:900]:  Audio FIFO Near Overflow raw = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:904]:IO map 0x83 = 0x62
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:905]:  Audio FIFO Near Underflow raw = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:906]:  Audio flat line = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:907]:  New audio samp freq = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:908]:  Audio parity error = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:909]:  Audio mode change raw = 0x20
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:917]:HDMI map 0x12 = 0x02
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:918]:  Audio FIFO almost empty threshold = 0x02
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:922]:HDMI map 0x11 = 0x7d
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:923]:  Audio FIFO almost full threshold = 0x7d
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:927]:HDMI map 0x18 = 0x31
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:928]:  Audio sample packet detect = 0x01
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:929]:  DSD packet detect = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:930]:  DST audio packet detect = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:931]:  HBR audio packet detect = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:935]:HDMI map 0x6E = 0x04
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:936]:  MUX_SPDIF_TO_I2S_ENABLE = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:940]:HDMI map 0x6D = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:941]:  I2S_SPDIF_MAP_ROT = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:942]:  I2S_SPDIF_MAP_INV = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:946]:HDMI map 0x03 = 0x90
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:947]:  I2SBITWIDTH = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:948]:  I2SOUTMODE = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:952]:IO map 0x65 = 0x4e
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:953]:  AUDIO_CH_MD_RAW = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:957]:HDMI map 0x07 = 0xa5
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:958]:  AUDIO_CHANNEL_MODE = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:962]:HDMI map 0x1A = 0x80
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:963]:  MUTE_AUDIO = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:964]:  NOT_AUTO_UNMUTE = 0x00
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:968]:HDMI map 0x0F = 0x1f
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:969]:  AUDIO_MUTE_SPEED = 0x0f
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:973]:IO map 0x65 = 0x4e
[2020-07-30 18:04:40 EDT]:[WRN]:[rap]:[libkx4_video]:[AdvChip.cpp:974]:  CS_DATA_VALID_RAW = 0x00

That last one seems important.  The thing is, when I connect an HDMI analyzer to the other branch of a splitter, it does seem to be receiving channel status, and as I said every other sink we connect to the Mac seems to have no trouble with the audio.

Would appreciate any suggestions on what to look at to sort this out.

Parents Reply Children
  • No, we don't.

    However, we have "sort of" isolated the problem based on this other Engineer Zone thread: https://ez.analog.com/video/f/q-a/119608/adv7619-audio-question.  Our situation appears to be identical to the one described there.

    As in that thread, clearing bits 2 and 3 of HDMI register 0x14 restore our audio.

    However, also like the original poster there, we don't understand the function of those two bits, and are uncertain whether it is safe to always clear them, or whether we only need to clear one of them, or what exactly.  A description is given for bit 2, but we also are not processing HDCP-encrypted content, so don't understand why that bit would be set.  And bit 3 remains a mystery.

    Can you shed any light on this?

  • Our ability to support custom hardware/software for the ADV7619 is very limited at this time. 

    If you could reproduce the issue on our ADV7619 evaluation board hardware/software, then we could rule out some issue with the custom hardware/software.

    -Matt