Ask for adv7481 HDMI YUV422 576p script

Can share me example script to enable HDMI to MIPI CSI 4-Lane with YUV422 8bit on 576p resolution by using adv7481?

Parents
  • Hi,

    720x480p60 and 720x576p50 are supported over 4 MIPI data lane in the YUV422 8-bit format. Please refer to table 81 in the hardware manual available here: ADV7481 Design Support Files 

    The script to use is :01-21 HDMI to MIPI TxA CSI 4-Lane - YUV422 8-Bit, Up to 600Mbps: in the ADV7481ES3C-VER.3.6c script file.

    Regarding the setting for Reg 0x40 in the HDMI RX Repeater Map, please refer to the HDCP specification. Bit 6 corresponds to the REPEATER bit in the Bcaps register. When you have this bit set, are you following the requirements for an HDCP repeater as described in the HDCP specification?

    Regards,

    Xavier

Reply
  • Hi,

    720x480p60 and 720x576p50 are supported over 4 MIPI data lane in the YUV422 8-bit format. Please refer to table 81 in the hardware manual available here: ADV7481 Design Support Files 

    The script to use is :01-21 HDMI to MIPI TxA CSI 4-Lane - YUV422 8-Bit, Up to 600Mbps: in the ADV7481ES3C-VER.3.6c script file.

    Regarding the setting for Reg 0x40 in the HDMI RX Repeater Map, please refer to the HDCP specification. Bit 6 corresponds to the REPEATER bit in the Bcaps register. When you have this bit set, are you following the requirements for an HDCP repeater as described in the HDCP specification?

    Regards,

    Xavier

Children
No Data