Can ADV7186 scale down the input video and able to drive a 1024x100 pix TFT LCD with RGB565 Formate?
Can ADV7186 scale down the input video and able to drive a 1024x100 pix TFT LCD with RGB565 Formate?
Hi,
The ADV7186 is under NDA so you will need to contact your local ADI sales / support team directly for support.
Best Regards,
Jeyasudha.M
Hi Hiberxen,
Do you have an answer on this question? I'm looking for a way to convert cvbs signal to parallel RGB565 for a small display of 320x240 pixels. Is the ADV7186 capable of doing this?
Looking forward to hear from you.
Best regards,
Robin
Hi,
As per the FUNCTIONAL BLOCK DIAGRAM of ADV7186 it can support cvbs input and it will output with 24 bit RGB
And also please refer the below link for different decoder with input/output support.
https://www.analog.com/en/product-category/video-decoders.html
Please find the below expert comments about for PAL to an RGB565
There are several ways to do this.
1) Use a YUV decoder like the ADV7280 and a CPLD on the output for color space conversion
2) Use a part like the ADV7842 and configure it's SDP Color Space Converter for YUV -> RGB
In both cases only use the high 5,6,5 bits from the RGB888 output"
NOTE: RGB565 is used to represent colours in 16 bits, rather than the 24bit (RGB888). RGB565 data is made up of RED (R = 5bits), GREEN (G = 6 bits), BLUE (B = 5 bits) to give overall 16 bits of digital inputs.
Thanks,
Poornima
What do you mean by "FUNCTIONAL BLOCK DIAGRAM"? So I can use the ADV7186 for this purpose? And is the 24-bit RGB in parallel? So RGB888 then?
I'm trying to obtain a proper datasheet for the ADV7186 from my local sales, however no datasheet so far....
Hi,
What do you mean by "FUNCTIONAL BLOCK DIAGRAM"? So I can use the ADV7186 for this purpose? And is the 24-bit RGB in parallel? So RGB888 then?
The block diagram you can find it in ADV7186 datasheet https://www.analog.com/media/en/technical-documentation/data-sheets/ADV7186.pdf
ADV7186 will support 24-bit RGB in parallel/RGB888.
I'm trying to obtain a proper datasheet for the ADV7186 from my local sales, however no datasheet so far....
ADV7186 is under NDA and to get complete datasheet or Manuals you will need to contact your local ADI sales/support team.
Thanks,
Poornima