Hi team,
My customer is now trying to change their design from ADV7320 to ADV7344 for new model because ADI do not recommend ADV7320 for new design. The customer used ADV7320 with ALSB=1 to enable I2C port filter becaus of they had faced I2C error from thir noisy system in past design. In the ADV7320 data sheet, this functionality is describe as below.
"When ALSB is set to 1, there is greater input bandwidth on the I2C lines, which allows high speed data transfers on this bus. When ALSB is set to 0, there is reduced input bandwidth on the I2C lines, which means that pulses of less than 50 ns do not pass into the I2C internal controller. This mode is recommended for noisy systems."
On the other hand, their is no description for I2C port filter in ADV7344 data sheet and the customer concern the ADV7344 I2C communication in their noisy system. What should customer do with ADV7344 in their system? Is external filter on I2C port needed if they want to have similar robustness from noise?
Regards,
Keiichi@ADKK