ADV7613
Recommended for New Designs
The ADV7613 is a high quality, low power, single-input HDMI
to LVDS display bridge. It incorporates an HDMI capable
receiver that supports up to 1080p...
Datasheet
ADV7613 on Analog.com
Hi !
It is the same person as this person with ID(donadona999s).
Something is wrong with my login information so I made another ID with my other mail address.
Sorry to confuse you.
I already asked about difference between ADV7613 and ADV7613-p.
(ADV7613)What is the difference between ADV7613WBBCZ & ADV7613WBBCZ-P?
And our customer are planing to use ADV7613.
SoC => HDMI => ADV7613 => oLDI
They don't need HDCP and DDC and Audio at their system.
My question is this.
Question)
When our customer don't need to use HDCP, what should they connect to these pins?
If OPEN is OK, please correct my comments.
***************************************************************************************************
・HPA_A
=> I think Pullup 1k to 5V is OK
Can they Pullup to 3.3V?
・RXA_5V
=> I think connect to 5V is OK
Can they Pullup to 3.3V?
・DDCA_SDA
=> I think OPEN or Pullup to 5V is OK.
Can they Pullup to 3.3V?
・DDCA_SCL
=> I think Pullup 47k to 5V is OK
Can they Pullup to 3.3V?
・Audio(AP0~AP5、SCLK、MCLKOUT)
=> I think OPEN is OK
・CEC
=> I think OPEN is OK
・CS
=> I think pull down 1k is OK.
***************************************************************************************************
Best regards
Kawa
Hi edo
Can they use 3.3V to pull-up?
best regards
Kawa
Hi edo
Can they use 3.3V to pull-up?
best regards
Kawa