Post Go back to editing

AD723 Input Resolution and format support

We are using DM388 SOC Display out which is connected to AD723 Encoder

What are the supported input resoltion for AD723?

We are Valitated the RGB out from DM388 to VGA conncetor it working fine.

The same RGB passed to AD723 for S-video conversion but We are not getting desired output

Connection:

DM388 -> THS7360 -> AD723 -> S-video display

AD723 Configuration:

4FSC - 14.31818MHz

TERM          - "0"
STND          - "1"
chip enable   - "1"
South America - "0"

Regards,

RAJM

Parents Reply Children
No Data