ADV7619 register setting

Hi~
According to the settings in the appendix: 02-08 720p, 1080i, 1080p In-36-bit RGB 444 Out:, the parameters at address 0x72 cannot be set.

:02-08 720p,1080i,1080p In - 36-bit RGB 444 Out:
98 FF 80 ; I2C reset
98 F4 80 ; CEC
98 F5 7C ; INFOFRAME
98 F8 4C ; DPLL
98 F9 64 ; KSV
98 FA 6C ; EDID
98 FB 68 ; HDMI
98 FD 44 ; CP
68 C0 03 ; ADI Required Write
98 01 06 ; Prim_Mode =110b HDMI-GR
98 02 F7 ; Auto CSC, RGB out, Set op_656 bit
98 03 42 ; 36 bit SDR 444 Mode 0
98 05 28 ; AV Codes Off
98 06 A6 ; Invert VS,HS pins
98 0C 42 ; Power up part
98 15 80 ; Disable Tristate of Pins
98 19 83 ; LLC DLL phase
98 33 40 ; LLC DLL MUX enable
44 BA 01 ; Set HDMI FreeRun
44 6C 00 ; Required ADI write
64 40 81 ; Disable HDCP 1.1 features
4C B5 01 ; Setting MCLK to 256Fs
68 C0 03 ; ADI Required write
68 00 08 ; Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)
68 02 03 ; ALL BG Ports enabled
68 03 98 ; ADI Required Write
68 10 A5 ; ADI Required Write
68 1B 08 ; ADI Required Write
68 45 04 ; ADI Required Write
68 97 C0 ; ADI Required Write
68 3D 10 ; ADI Required Write
68 3E 69 ; ADI Required Write
68 3F 46 ; ADI Required Write
68 4E FE ; ADI Required Write
68 4F 08 ; ADI Required Write
68 50 00 ; ADI Required Write
68 57 A3 ; ADI Required Write
68 58 07 ; ADI Required Write
68 6F 08 ; ADI Required Write
68 83 FC ; Enable clock terminators for port A & B
68 84 03 ; ADI Required Write
68 85 10 ; ADI Required Write
68 86 9B ; ADI Required Write
68 89 03 ; ADI Required Write
68 9B 03 ; ADI Required Write
68 93 03 ; ADI Required Write
68 5A 80 ; ADI Required Write
68 9C 80 ; ADI Required Write
68 9C C0 ; ADI Required Write
68 9C 00 ; ADI Required Write
72 01 00 ; Set N Value(6144)
72 02 18 ; Set N Value(6144)
72 03 00 ; Set N Value(6144)
72 15 00 ; Input 444 (RGB or YCrCb) with Separate Syncs, 44.1kHz fs
72 16 61 ; RGB 444
72 18 46 ; CSC disabled
72 3B 80 ; PR Auto Mode
72 40 80 ; General Control Packet Enable
72 41 10 ; Power Down control
72 48 08 ; Data right justified
72 49 A8 ; Set Dither_mode - 12-to-10 bit
72 4C 06 ; 12 bit Output
72 55 00 ; Set RGB in AVinfo Frame
72 56 08 ; Set active format Aspect
72 96 20 ; HPD Interrupt clear
72 98 03 ; ADI Required Write
72 99 02 ; ADI Required Write
72 9C 30 ; PLL Filter R1 Value
72 9D 61 ; Set clock divide
72 A2 A4 ; ADI Required Write
72 A3 A4 ; ADI Required Write
72 AF 16 ; Set HDMI Mode
72 BA 60 ; No clock delay
72 DE 9C ; ADI Required Write
72 E4 60 ; VCO Swing Reference Voltage
72 FA 7D ; Nbr of times to search for good phase
End

Parents Reply Children
No Data