Post Go back to editing

HDMI to CVBS conversion

Thread Summary

The user inquired about converting HDMI to CVBS using ADV7611 and ADV7393. The final answer confirmed this as a viable solution, recommending the use of 22 or 33 Ohm resistors for HDMI traces and ensuring clean 1.8V power rails with LC filters. The DAC output of the ADV7393 should use a 75 Ohm series resistor and a 75 Ohm load resistor. The user was also advised to cross-check the schematic with the ADV7611 and ADV7393 design support files.
AI Generated Content

Hello.

I found a way to convert HDMI to CVBS with two chips: HDMI->ADV7611->ADV7393->CVBS

Is this the easiest and cheapest solution?

Parents Reply Children