I am using ADV7625ES2C.xml in AVES3_EVAL-ADV7625-SMZ_20160127.
However, there is no tab to set the EDID applied to input.
How do I apply?
Do I need to define it myself?
ADV7525
Production
The ADV7525 is an 80 MHz, high definition multimedia
interface (HDMI®) transmitter with expanded CEC buffer. It supports HDTV formats up to 1080i and computer...
Datasheet
ADV7525 on Analog.com
I am using ADV7625ES2C.xml in AVES3_EVAL-ADV7625-SMZ_20160127.
However, there is no tab to set the EDID applied to input.
How do I apply?
Do I need to define it myself?
Hi,
The XML file is only needed if you want to read/write registers using the graphical interface of AVES3.
If you use our software driver to configure the board, then our repeater function will just copy the EDID from sink which is connected to TX into the RX which is connected to the source.
Note: If you are using consumer electronic devices as a source (rather than a DVI/HDMI generator), You will need to ensure that the ADV7625 is configured with an appropriate EDID.The SW driver copies the sink's EDID from TX memory to the RX memory whereas the scripts do not.
Below is the example for how to use EDID in the script.
Here is a script to configure the ADV7625 with the EDID from an LG 84" TV. You can copy this into your scripts file.
##11 Sample EDID##
:11-01-02 EDID data from LG 84 inch:
B0 ED 6C ; default=0x00, Set EDID address
B0 EE 64 ; default=0x00, Set Rx1_Repeater_Map address
64 74 00 ; Disable the Internal EDID for all ports
6C 00 00
6C 01 FF
6C 02 FF
6C 03 FF
6C 04 FF
6C 05 FF
6C 06 FF
6C 07 00
6C 08 1E
6C 09 6D
6C 0A 01
6C 0B 00
6C 0C 01
6C 0D 01
6C 0E 01
6C 0F 01
6C 10 01
6C 11 16
6C 12 01
6C 13 03
6C 14 80
6C 15 A0
6C 16 5A
6C 17 78
6C 18 0A
6C 19 EE
6C 1A 91
6C 1B A3
6C 1C 54
6C 1D 4C
6C 1E 99
6C 1F 26
6C 20 0F
6C 21 50
6C 22 54
6C 23 A1
6C 24 08
6C 25 00
6C 26 31
6C 27 40
6C 28 45
6C 29 40
6C 2A 61
6C 2B 40
6C 2C 71
6C 2D 40
6C 2E 81
6C 2F 80
6C 30 01
6C 31 01
6C 32 01
6C 33 01
6C 34 01
6C 35 01
6C 36 02
6C 37 3A
6C 38 80
6C 39 18
6C 3A 71
6C 3B 38
6C 3C 2D
6C 3D 40
6C 3E 58
6C 3F 2C
6C 40 45
6C 41 00
6C 42 A0
6C 43 5A
6C 44 00
6C 45 00
6C 46 00
6C 47 1E
6C 48 66
6C 49 21
6C 4A 50
6C 4B B0
6C 4C 51
6C 4D 00
6C 4E 1B
6C 4F 30
6C 50 40
6C 51 70
6C 52 36
6C 53 00
6C 54 A0
6C 55 5A
6C 56 00
6C 57 00
6C 58 00
6C 59 1E
6C 5A 00
6C 5B 00
6C 5C 00
6C 5D FD
6C 5E 00
6C 5F 3A
6C 60 3E
6C 61 1E
6C 62 53
6C 63 10
6C 64 00
6C 65 0A
6C 66 20
6C 67 20
6C 68 20
6C 69 20
6C 6A 20
6C 6B 20
6C 6C 00
6C 6D 00
6C 6E 00
6C 6F FC
6C 70 00
6C 71 4C
6C 72 47
6C 73 20
6C 74 54
6C 75 56
6C 76 0A
6C 77 20
6C 78 20
6C 79 20
6C 7A 20
6C 7B 20
6C 7C 20
6C 7D 20
6C 7E 01
6C 7F 43
6C 80 02
6C 81 03
6C 82 31
6C 83 F1
6C 84 48
6C 85 90
6C 86 22
6C 87 20
6C 88 05
6C 89 04
6C 8A 03
6C 8B 02
6C 8C 01
6C 8D 23
6C 8E 09
6C 8F 57
6C 90 07
6C 91 7B
6C 92 03
6C 93 0C
6C 94 00
6C 95 10
6C 96 00
6C 97 B8
6C 98 3C
6C 99 20
6C 9A C0
6C 9B 6E
6C 9C 01
6C 9D 02
6C 9E 03
6C 9F 01
6C A0 4F
6C A1 00
6C A2 FE
6C A3 08
6C A4 10
6C A5 06
6C A6 10
6C A7 18
6C A8 10
6C A9 28
6C AA 10
6C AB 38
6C AC 10
6C AD E3
6C AE 05
6C AF 03
6C B0 01
6C B1 02
6C B2 3A
6C B3 80
6C B4 18
6C B5 71
6C B6 38
6C B7 2D
6C B8 40
6C B9 58
6C BA 2C
6C BB 45
6C BC 00
6C BD A0
6C BE 5A
6C BF 00
6C C0 00
6C C1 00
6C C2 1E
6C C3 01
6C C4 1D
6C C5 80
6C C6 18
6C C7 71
6C C8 1C
6C C9 16
6C CA 20
6C CB 58
6C CC 2C
6C CD 25
6C CE 00
6C CF A0
6C D0 5A
6C D1 00
6C D2 00
6C D3 00
6C D4 9E
6C D5 01
6C D6 1D
6C D7 00
6C D8 72
6C D9 51
6C DA D0
6C DB 1E
6C DC 20
6C DD 6E
6C DE 28
6C DF 55
6C E0 00
6C E1 A0
6C E2 5A
6C E3 00
6C E4 00
6C E5 00
6C E6 1E
6C E7 26
6C E8 36
6C E9 80
6C EA A0
6C EB 70
6C EC 38
6C ED 1F
6C EE 40
6C EF 30
6C F0 20
6C F1 25
6C F2 00
6C F3 A0
6C F4 5A
6C F5 00
6C F6 00
6C F7 00
6C F8 1A
6C F9 00
6C FA 00
6C FB 00
6C FC 00
6C FD 00
6C FE 00
6C FF B1
64 74 1F ; Enable the Internal EDID for RXA/RXB/RXC/RXD/RXE
Thanks,
Poornima
Hi,
The XML file is only needed if you want to read/write registers using the graphical interface of AVES3.
If you use our software driver to configure the board, then our repeater function will just copy the EDID from sink which is connected to TX into the RX which is connected to the source.
Note: If you are using consumer electronic devices as a source (rather than a DVI/HDMI generator), You will need to ensure that the ADV7625 is configured with an appropriate EDID.The SW driver copies the sink's EDID from TX memory to the RX memory whereas the scripts do not.
Below is the example for how to use EDID in the script.
Here is a script to configure the ADV7625 with the EDID from an LG 84" TV. You can copy this into your scripts file.
##11 Sample EDID##
:11-01-02 EDID data from LG 84 inch:
B0 ED 6C ; default=0x00, Set EDID address
B0 EE 64 ; default=0x00, Set Rx1_Repeater_Map address
64 74 00 ; Disable the Internal EDID for all ports
6C 00 00
6C 01 FF
6C 02 FF
6C 03 FF
6C 04 FF
6C 05 FF
6C 06 FF
6C 07 00
6C 08 1E
6C 09 6D
6C 0A 01
6C 0B 00
6C 0C 01
6C 0D 01
6C 0E 01
6C 0F 01
6C 10 01
6C 11 16
6C 12 01
6C 13 03
6C 14 80
6C 15 A0
6C 16 5A
6C 17 78
6C 18 0A
6C 19 EE
6C 1A 91
6C 1B A3
6C 1C 54
6C 1D 4C
6C 1E 99
6C 1F 26
6C 20 0F
6C 21 50
6C 22 54
6C 23 A1
6C 24 08
6C 25 00
6C 26 31
6C 27 40
6C 28 45
6C 29 40
6C 2A 61
6C 2B 40
6C 2C 71
6C 2D 40
6C 2E 81
6C 2F 80
6C 30 01
6C 31 01
6C 32 01
6C 33 01
6C 34 01
6C 35 01
6C 36 02
6C 37 3A
6C 38 80
6C 39 18
6C 3A 71
6C 3B 38
6C 3C 2D
6C 3D 40
6C 3E 58
6C 3F 2C
6C 40 45
6C 41 00
6C 42 A0
6C 43 5A
6C 44 00
6C 45 00
6C 46 00
6C 47 1E
6C 48 66
6C 49 21
6C 4A 50
6C 4B B0
6C 4C 51
6C 4D 00
6C 4E 1B
6C 4F 30
6C 50 40
6C 51 70
6C 52 36
6C 53 00
6C 54 A0
6C 55 5A
6C 56 00
6C 57 00
6C 58 00
6C 59 1E
6C 5A 00
6C 5B 00
6C 5C 00
6C 5D FD
6C 5E 00
6C 5F 3A
6C 60 3E
6C 61 1E
6C 62 53
6C 63 10
6C 64 00
6C 65 0A
6C 66 20
6C 67 20
6C 68 20
6C 69 20
6C 6A 20
6C 6B 20
6C 6C 00
6C 6D 00
6C 6E 00
6C 6F FC
6C 70 00
6C 71 4C
6C 72 47
6C 73 20
6C 74 54
6C 75 56
6C 76 0A
6C 77 20
6C 78 20
6C 79 20
6C 7A 20
6C 7B 20
6C 7C 20
6C 7D 20
6C 7E 01
6C 7F 43
6C 80 02
6C 81 03
6C 82 31
6C 83 F1
6C 84 48
6C 85 90
6C 86 22
6C 87 20
6C 88 05
6C 89 04
6C 8A 03
6C 8B 02
6C 8C 01
6C 8D 23
6C 8E 09
6C 8F 57
6C 90 07
6C 91 7B
6C 92 03
6C 93 0C
6C 94 00
6C 95 10
6C 96 00
6C 97 B8
6C 98 3C
6C 99 20
6C 9A C0
6C 9B 6E
6C 9C 01
6C 9D 02
6C 9E 03
6C 9F 01
6C A0 4F
6C A1 00
6C A2 FE
6C A3 08
6C A4 10
6C A5 06
6C A6 10
6C A7 18
6C A8 10
6C A9 28
6C AA 10
6C AB 38
6C AC 10
6C AD E3
6C AE 05
6C AF 03
6C B0 01
6C B1 02
6C B2 3A
6C B3 80
6C B4 18
6C B5 71
6C B6 38
6C B7 2D
6C B8 40
6C B9 58
6C BA 2C
6C BB 45
6C BC 00
6C BD A0
6C BE 5A
6C BF 00
6C C0 00
6C C1 00
6C C2 1E
6C C3 01
6C C4 1D
6C C5 80
6C C6 18
6C C7 71
6C C8 1C
6C C9 16
6C CA 20
6C CB 58
6C CC 2C
6C CD 25
6C CE 00
6C CF A0
6C D0 5A
6C D1 00
6C D2 00
6C D3 00
6C D4 9E
6C D5 01
6C D6 1D
6C D7 00
6C D8 72
6C D9 51
6C DA D0
6C DB 1E
6C DC 20
6C DD 6E
6C DE 28
6C DF 55
6C E0 00
6C E1 A0
6C E2 5A
6C E3 00
6C E4 00
6C E5 00
6C E6 1E
6C E7 26
6C E8 36
6C E9 80
6C EA A0
6C EB 70
6C EC 38
6C ED 1F
6C EE 40
6C EF 30
6C F0 20
6C F1 25
6C F2 00
6C F3 A0
6C F4 5A
6C F5 00
6C F6 00
6C F7 00
6C F8 1A
6C F9 00
6C FA 00
6C FB 00
6C FC 00
6C FD 00
6C FE 00
6C FF B1
64 74 1F ; Enable the Internal EDID for RXA/RXB/RXC/RXD/RXE
Thanks,
Poornima