Post Go back to editing

ADV7619 HPA hardware failure

Hi all!

We've a custom hardware using a ADV7619 in prototyping stage where the second board just failed due to HPA not going high. (It was working for some time.) I'd like to find out why that happens. Our schematic followes the reference design (RXA_5V via 1k to HPA_A, RXA_5V and HPA_A directly connected to ADV, HPA connected to external ESD protection). On the dead hardware we found, that HPA does not raise above 1.7V. If we cut the wire between the 1k and HPA, HPA raises (because its not controlled by the ADV anymore) but SDA is kept low.

The register programming does not follow the recommendations yet. We've configured HPA_AUTO_INT_EDID to mode 2 (HPA goes high if EDID is active and after cable detect delay, HDMI reg 0x6C, bits 1 and 2) and disable the DDC/EDID via Repeater reg. 74 bits 0 and 1 while changing the EDID memory.

Does anymore have an idea why HPA does not work in our setup?

Best regards

Pauliman