ADV7181C - RGB to 422 EAV/SAV

Hello,

Right now we are testing the ADV7181C on the EVAL-ADV7181CEBZ board. For that we are using the ADV Register Control program (Version 3.56) and the sample script version 3.2c.

Unfortunately the sample script does not offer the option RGB (as input) and 422 EAV/SAV (as output) using the color space converter.

Is there maybe a new version for the sample script that offers that? Or are there other resources we can use to test that?

Thanks.

Sincerly

Peter Hildebrandt

Parents
  • Hello,

    In addition to the ADV7181C-evalboard

      we have prototypes of our own design with the ADV7181C as well.

    So we can use these to test the desired mode.

    Any help and input on finding register settings to test XGA-in and YCbCr-out

      on our prototypes is greatly appreciated.

    Thanks,

    Peter

    --- desired mode ----------------

    IN: RGB XGA 1024x768 @ 60Hz with ext. hsync and vsync

    OUT: YCbCr 16bit 422 EAV/SAV

Reply
  • Hello,

    In addition to the ADV7181C-evalboard

      we have prototypes of our own design with the ADV7181C as well.

    So we can use these to test the desired mode.

    Any help and input on finding register settings to test XGA-in and YCbCr-out

      on our prototypes is greatly appreciated.

    Thanks,

    Peter

    --- desired mode ----------------

    IN: RGB XGA 1024x768 @ 60Hz with ext. hsync and vsync

    OUT: YCbCr 16bit 422 EAV/SAV

Children
No Data