ADV7181C - RGB to 422 EAV/SAV

Hello,

Right now we are testing the ADV7181C on the EVAL-ADV7181CEBZ board. For that we are using the ADV Register Control program (Version 3.56) and the sample script version 3.2c.

Unfortunately the sample script does not offer the option RGB (as input) and 422 EAV/SAV (as output) using the color space converter.

Is there maybe a new version for the sample script that offers that? Or are there other resources we can use to test that?

Thanks.

Sincerly

Peter Hildebrandt

Parents
  • Hi Peter,

    Unfortunately, there is no script available to configure the EVAL-ADV7181CEBZ board for a RGB XGA @60Hz input, with the ADV7181C configured to output YCbCr 16bit 422 EAV/SAV. The encoder will not support such an XGA @60Hz type of resolution, and only 12 output bits from the ADV7181C are connected to HDMI transmitter.

    Xavier

Reply
  • Hi Peter,

    Unfortunately, there is no script available to configure the EVAL-ADV7181CEBZ board for a RGB XGA @60Hz input, with the ADV7181C configured to output YCbCr 16bit 422 EAV/SAV. The encoder will not support such an XGA @60Hz type of resolution, and only 12 output bits from the ADV7181C are connected to HDMI transmitter.

    Xavier

Children
No Data