ADV7181C
Production
The ADV7181C is a high quality, single-chip, multiformat video decoder and graphics digitizer. This multiformat decoder supports the conversion of PAL...
Datasheet
ADV7181C on Analog.com
ADV7128
Obsolete
The ADV7128 (ADV®) is a video speed, digital-to-analog converter on a single monolithic chip. It consists of a high speed, 10-bit, video D/A converter;...
Datasheet
ADV7128 on Analog.com
I have a customer looking to capture RS-343 video (high resolution monochrome composite video used primarily in mil/aero) and wanted to know if we have any parts that have been used to do this? I was thinking maybe the ADV7181C could do the job but am looking for some sort history that the part can be setup correctly for this standard?
I also noticed the ADV7128 supports RS-343 as an output, so there must be a complimentary part to bring the signal in? Any insight would be useful as I am relatively new to the line... Thanks!!
I can’t find a lot about EIA 343 in terms of what exactly the details are. It is a monochrome high definition spec. This is what I did find:
RS-343 was introduced later than RS-170 and intended, according to the title, as a signal standard for "high-definition closed-circuit television", which among other things reduced the signal amplitude to 1.00 Vp-p. The signal specifications according RS-343:
White: +0.714V Black: +0.054V Blank: (0V reference) Sync: -0.286V.
RS-343 specifies a 60 Hz non-interlaced scan with a composite sync signal with timings that produce a non-interlace (progressive) scan at 675 to 1023 lines.
This standard is used by some computer systems and high resolution video cameras. Precision imaging systems, infrared targeting, low-light TV, night-vision and special military display systems, usually operate to high-resolution, RS-343 standards (875-line, 30-frame scan). They require specialized and costly recording and display equipment.
Given that, our parts are, in general, color. You can decode to Y Cr Cb and only use the Y component. There are no scripts available specifically for EIA 343.
I've seen this question before fairly recently. My understanding is that none of our video decoder parts decode this format. RS-170, yes but not RS-343.
If you separated the synch off and just fed it into Y, I imagine you could do it using the CP of most of or video decoder parts. I'm not aware of anyone who has tried though.
Dave
Dave,
I know this thread is over 2 years old, so I'm wondering if this is still the case (that AD "does not" have any RS-343 solution)? We have a board that is using the ADV7842, so I was hoping that we could tweak that to accept RS-343 (875 line resolution), but another solution could prove interesting.
Please advise.
Hi Rob,
Nope, we have not made any changes in support for RS-343. There hasn't been any indication that there is enough business out there to justify the development unfortunately.
Dave