Post Go back to editing

Encode a large pixels in ADV202/ADV212

Hi,

I am finding method to encode a large pixel (width 2000x height 3000) in ADV202/212.

I received a suggestion pixel shall be divided by 6 tiles (1tile= 2000 x 500) in the previous thred.

But i can not understand how to input 6 tile and can ADV202 encode automatically.

Let tell me register setting.

Kubo

Parents
  • Hi Dave,

    We also need to encode an image with total samples (1440x900=1.3M or 2.6M for YCbCr 4:2:2) larger than both the 1.048 Msamples/image limit in Custom Specific mode and the max tile sizes suppported.  Our output will be saved to a file(s) and ultimately viewed using a software decoder.

    Can you please elaborate on your last response.  When you suggest keeping the codestreams separate, does that mean using raw mode with separate ADV212 chips (or making three passes with one chip if the data rate permits) for each component?  Will each separate component input still need to be separated into tiles?  How many different codestreams per image will be created and merged on the PC side for decode?  Can you provide more details on how they are merged on the PC side for decode?  Finally, is there an advantage to working in either RGB or YCbCr input format for this example?  My input is in RGB but I can change to YCbCr or YCbYCr 4:2:2 if it helps.

    Thanks,

    Keith,

Reply
  • Hi Dave,

    We also need to encode an image with total samples (1440x900=1.3M or 2.6M for YCbCr 4:2:2) larger than both the 1.048 Msamples/image limit in Custom Specific mode and the max tile sizes suppported.  Our output will be saved to a file(s) and ultimately viewed using a software decoder.

    Can you please elaborate on your last response.  When you suggest keeping the codestreams separate, does that mean using raw mode with separate ADV212 chips (or making three passes with one chip if the data rate permits) for each component?  Will each separate component input still need to be separated into tiles?  How many different codestreams per image will be created and merged on the PC side for decode?  Can you provide more details on how they are merged on the PC side for decode?  Finally, is there an advantage to working in either RGB or YCbCr input format for this example?  My input is in RGB but I can change to YCbCr or YCbYCr 4:2:2 if it helps.

    Thanks,

    Keith,

Children
No Data