Hello,
I'm wondering how many transistor and/or effective gates are in the AD8048 and AD8031.
Thank you for any information might be available and happy new year
AD8048
Production
The AD8047 and AD8048 are very high speed and wide bandwidth amplifiers. The AD8047 is unity gain stable. The AD8048 is stable at gains of two or greater...
Datasheet
AD8048 on Analog.com
AD8031
Production
The AD8031 (single) is a single supply voltage feedback amplifier that features high speed performance with 80 MHz of small signal bandwidth, 30 V/µs...
Datasheet
AD8031 on Analog.com
Hello,
I'm wondering how many transistor and/or effective gates are in the AD8048 and AD8031.
Thank you for any information might be available and happy new year
Hi Derek,
May I know why would be needing the numbers? Is it for reliability? If so, we provide FIT numbers for the Integrated circuit that you can use. See:
https://www.analog.com/en/about-adi/quality-reliability/reliability-data/wafer-fabrication-data.html
I am currently in contact with the designer for the data needed. I'll post it ASAP once available.
Regards,
Goz
Hi Gauzz,
I am modeling expected upset rates in various radiation environments. I don't need the exact number of transistors. To a factor of 10 is sufficient for my purpose. The FIT number is useful in a separate reliability analysis but for this portion I am looking for a rough estimate of transistors.
I appreciate your help.
Hi Derek,
For AD8031 the transistor count should be 98, and for AD8048 should be around that number too. Typically, General Op Amps would have 100 transistors in them.
Apologies for getting back late.
Best Regards,
Goz
Much appreciated. This is just what I was looking for.