Hi ADI's
One of my customers is reviewing product development using the ADV7343.
RS170 (640 x 480,30fps), 4 channels of black and white video are used in Black Bar mode.
would like to implement the structure below.
1. Should the DAC1 ~ 3 be directly connected to the datasheet of the ADV7343 by BNC, and should the DAC4 ~ 6 be connected to the BNC using Amp?
2. Can I use ADA4432 as an amp when using DAC 4 ~ 6?
3. Should test pattern occur one by one when DAC1 ~ 4 occurs? Or can it happen at the same time?
Thank you