Post Go back to editing

ADV7179 Colour bar mode problem

I have some problem with ADV7179 Colour bar mode. I set the MR17 bit

Setting this bit did not change anything. I can not get anything out of ADV7179. I use the subcarrier frequency register set provided in the datasheet for PAL B/D/G/H/I (FSC = 4.43361875 MHz). I use CVBS on DAC B.

Here is the procedure I use: Power> toggle reset pin>transfer register datas via I2C by microBlaze CPU> toggle TR07 bit by sending TR0 data via I2C 2 times(first TR07=1, the second TR07=0). and I get nothing on the screen. Please provide a extact register set for colorbar test and extact timing for reset times. There is no problem with hardware since it is provided by xilinx. Here are the output waveforms of the DAC B on osciloscope:

Here is the register data I used:

(first I send 0x00 for address register, then I send these datas cont.)

Mode Register 0 = 0x65h

Mode Register 1 = 0x11h

Mode Register 2 = 0x00h

Mode Register 3 = 0x0Ch

Mode Register 4 = 0x22h

RESERVED = 0x00h

RESERVED = 0x00h

Timing Register 0 = 0x01h  (TR07=1)

Timing Register 1 = 0x00h

Subcarrier Frequency Register 0 = 0xCBh

Subcarrier Frequency Register 1 = 0x8Ah

Subcarrier Frequency Register 2 = 0x09h

Subcarrier Frequency Register 3 = 0x2Ah

Subcarrier Phase Register and the rest of them = 0x00

After sending these datas, I send TR0 againg for toggling TR07 bit: I first send 0x07 for address of TR0 and then 0x81 (TR07=1), then I send 0x07 for address of TR0 and 0x01 (TR07=0).

Is there any problem?

Is there any problem with transmitting RESERVED register datas with 0x00? Or I should program the first 5 registers and generate and STOP condition, and after that sen the address=0x07 to point to the TR0 and then send the remaining register datas?

These information are not provided in the datasheet, and there is NO application note for this device!

Please Help.

Parents
  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
  • HI All,

    I was facing the same issue with ADV7179(Some colors are missing,when we enable bar pattern.)

    Input clock frequency to ADV7179 - 27MHz from FPGA.

    Voltage levels are proper,Ref voltage to ADV7179 - 1.22V.

    I am getting all the I2C read ack when i was writing into registers.

    Below are the registers we are configuring.

    #define I2C_MODE_0_VAL      0x45
    #define I2C_MODE_1_VAL      0xB8
    #define I2C_MODE_2_VAL      0x00
    #define I2C_MODE_3_VAL      0x80
    #define I2C_MODE_4_VAL      0x08
    #define I2C_TIME_0_VAL        0x05
    #define I2C_TIME_1_VAL        0x02

    #define I2C_TIMERESET_VAL    0x89
    #define I2C_SUB_FREQ_0_VAL    0xCB
    #define I2C_SUB_FREQ_1_VAL    0x8A


    /* Clear test pattern */
    #define I2C_SUB_FREQ_2_VAL    0x09
    /* Exit Power-down mode */
    #define I2C_SUB_FREQ_3_VAL    0x2A
    #define I2C_SUB_PHASE_VAL   0x00
    /* Monitor polarity is handled via DVI Sync Polarity Register */
    #define I2C_DVI_SYNC_POLARITY_VAL        0x00


    What i want was PAL resolution internal color bar composite on channel A.

    Output of DAC connected to TV.

    The same reference design provided in ADV7179 datasheet, i was using.

    when i play the actual video on DAC A instead Color bar.Only proper color i can see in the screen was from 70% to 100%. Remaining 0 to 70% is fixed color was light green always fixed in that area.

    The same problem with internal color bar pattern also.

    Please help me out.

Reply
  • HI All,

    I was facing the same issue with ADV7179(Some colors are missing,when we enable bar pattern.)

    Input clock frequency to ADV7179 - 27MHz from FPGA.

    Voltage levels are proper,Ref voltage to ADV7179 - 1.22V.

    I am getting all the I2C read ack when i was writing into registers.

    Below are the registers we are configuring.

    #define I2C_MODE_0_VAL      0x45
    #define I2C_MODE_1_VAL      0xB8
    #define I2C_MODE_2_VAL      0x00
    #define I2C_MODE_3_VAL      0x80
    #define I2C_MODE_4_VAL      0x08
    #define I2C_TIME_0_VAL        0x05
    #define I2C_TIME_1_VAL        0x02

    #define I2C_TIMERESET_VAL    0x89
    #define I2C_SUB_FREQ_0_VAL    0xCB
    #define I2C_SUB_FREQ_1_VAL    0x8A


    /* Clear test pattern */
    #define I2C_SUB_FREQ_2_VAL    0x09
    /* Exit Power-down mode */
    #define I2C_SUB_FREQ_3_VAL    0x2A
    #define I2C_SUB_PHASE_VAL   0x00
    /* Monitor polarity is handled via DVI Sync Polarity Register */
    #define I2C_DVI_SYNC_POLARITY_VAL        0x00


    What i want was PAL resolution internal color bar composite on channel A.

    Output of DAC connected to TV.

    The same reference design provided in ADV7179 datasheet, i was using.

    when i play the actual video on DAC A instead Color bar.Only proper color i can see in the screen was from 70% to 100%. Remaining 0 to 70% is fixed color was light green always fixed in that area.

    The same problem with internal color bar pattern also.

    Please help me out.

Children
No Data