ADV7842 CVBS to RGB Out

I've been using the AVES scripts for the ADV7842/AD7511 eval board to successfully setup up my custom ADV7842 board to handle analog RGB inputs.  I've moved onto CVBS (NTSC) inputs and I'm not having the same success.  I started with the 1-1e script (NTSC to 480i HDMI) and I was able to get video out of my board but the colors where all messed up.  Specifically, black is coming out as purple and white is coming out as a lime color.  As I dug into it I saw the script sets up the ADV7511 to accept YCrCb so the ADV7842 must output YCrCb.  However, the DVI Transmitter on my board only accepts RGB so I need the ADV7842 to output RGB as it did with the analog RGB input scripts.  I thought that should be as simple as switching 0x40 (IO) 0x02[1] from '0' to '1' but that seemed to have no impact.  I realize the analog RGB inputs use CP and the CVBS inputs use SDP but other than the register I just mentioned I don't see anything related to SDP color output specifically.

I've been analyzing scripts all day and I can't seem to figure out why the analog RGB input scripts work but the CVBS input scripts don't.  Do you have any ideas or things for me to check that might help me diagnose because I'm pretty stumped?

By the way, I tried disabling the 3D comb filter to take the SDRAM on my board out of the equation and it didn't resolve my issue.

Thanks,

Nathan

Parents
  • This seemed to be a step in the right direction.  Black is now black but all other colors are now a different shade of green.  Below is what I added to my script:

    write 0x94 0xE0 0x08
    write 0x94 0xE1 0x00
    write 0x94 0xE2 0x1A
    write 0x94 0xE3 0x6A
    write 0x94 0xE4 0x1D
    write 0x94 0xE5 0x50
    write 0x94 0xE6 0x04
    write 0x94 0xE7 0x23
    write 0x94 0xE8 0x08
    write 0x94 0xE9 0x00
    write 0x94 0xEA 0x0A
    write 0x94 0xEB 0xF8
    write 0x94 0xEC 0x00
    write 0x94 0xED 0x00
    write 0x94 0xEE 0x1A
    write 0x94 0xEF 0x84
    write 0x94 0xF0 0x08
    write 0x94 0xF1 0x00
    write 0x94 0xF2 0x00
    write 0x94 0xF3 0x00
    write 0x94 0xF4 0x0D
    write 0x94 0xF5 0xDB
    write 0x94 0xF6 0x19

Reply
  • This seemed to be a step in the right direction.  Black is now black but all other colors are now a different shade of green.  Below is what I added to my script:

    write 0x94 0xE0 0x08
    write 0x94 0xE1 0x00
    write 0x94 0xE2 0x1A
    write 0x94 0xE3 0x6A
    write 0x94 0xE4 0x1D
    write 0x94 0xE5 0x50
    write 0x94 0xE6 0x04
    write 0x94 0xE7 0x23
    write 0x94 0xE8 0x08
    write 0x94 0xE9 0x00
    write 0x94 0xEA 0x0A
    write 0x94 0xEB 0xF8
    write 0x94 0xEC 0x00
    write 0x94 0xED 0x00
    write 0x94 0xEE 0x1A
    write 0x94 0xEF 0x84
    write 0x94 0xF0 0x08
    write 0x94 0xF1 0x00
    write 0x94 0xF2 0x00
    write 0x94 0xF3 0x00
    write 0x94 0xF4 0x0D
    write 0x94 0xF5 0xDB
    write 0x94 0xF6 0x19

Children
No Data