Post Go back to editing

ADV7511 works with SPDIF audio in 480p 60Hz but not 576p 50Hz video modes

Thread Summary

The user encountered an issue with the ADV7511 where 576p 50Hz video mode stopped working when SPDIF audio was enabled. The problem was resolved by ensuring the video source did not send pixel data during the VSYNC period. No known errata was mentioned, but the user is interested in hearing if others have faced similar issues.
AI Generated Content

We are using the ADV7511 to provide HDMI video+audio for a computing device. 

This works fine for 480p 60Hz and for 576p 50Hz, if we have no audio. 

However, if we enable the SPDIF audio (at any sample rate), then the 576p 50Hz video mode stops working, i.e., the monitor acts as though there is no signal.

This does not occur if we are using the 480p 60Hz video mode.

ADV7511 I2C main map register values:

:00:140031001000000000001D8E00180113
:10:2537200000F03000466204A800001C00
:20:1CBF04A81E70021E000004A808121BAC
:30:00000000000000000000008011114400
:40:C010707E7970000010A8800004000000
:50:0000020D001219000000000000000000
:60:00000000000000000000000000000000
:70:010A0001000000000000000000000000
:80:00000000000000000000000000000000
:90:00000000C00024800302E01830611100
:A0:0000A4A4080400000000004000004002
:B0:00000000000000000000000000000000
:C0:00000000009006004202000002000104
:D0:3CFF8080800000000000000000001001
:E0:D0780000600000000000000000000000
:F0:0000000000751100000000005D000156

Is this a known errata, or is there something Bleeding Obvious that we haven't got right?

Any suggestions of leads to follow up would be most appreciated.

Paul.