Question from customer:
How can I use ADV7611 with an internal EDID?
ADV7611
Recommended for New Designs
The ADV7611 is offered in automotive, professional (no HDCP), and industrial versions. The operating temperature range is −40°C to +85°C.
The UG-180...
Datasheet
ADV7611 on Analog.com
Question from customer:
How can I use ADV7611 with an internal EDID?
Sure, but it is still relevant, i.e., I haven't found a thread that seems to resolve the EDID issue with adv7611
So far these ones are relevant:
ADV7611: Internal EDID stays disabled (as above)
(ADV7611) To enable internal EDID. (marked as answered, but with no answer given)
Sure, but it is still relevant, i.e., I haven't found a thread that seems to resolve the EDID issue with adv7611
So far these ones are relevant:
ADV7611: Internal EDID stays disabled (as above)
(ADV7611) To enable internal EDID. (marked as answered, but with no answer given)