Post Go back to editing

Recommended inductor for Y-TRAP of AD725

Inductor devices do have more properties than just an inductance.

Datasheet, evaluation board document and other resources I find on the internet do not give any idea other than 68 uH inductance. Here's a pic of possibly well performing inductor:

The one almost at the center marked 680J is expected to be the required inductor, its length must be 2.1 mm (comparing to the size of AD725), but I can not find such inductors.

I would appreciate if AD people would give part numbers of recommended (or successfully used) inductors, and then I will find out my way to source appropriate one locally.

Thank you.

Update: (after Guenter's reply)

The board in the picture above is Altium "12-404-PB01 -  Audio/Video Peripheral Board, Provides a Stereo Audio CODEC, 24-Bit VGA Output", here's the circuit diagram

PDF

The document does not list the BOM, but each component has more or less complete characteristic written on. For Y-trap inductor it has "68uH 80mA 5.5R" title, thus it is very close to the Guenter's proposed part.

Update: here's the final product based on the AD725.



added final product image
[edited by: Eugeny Brychkov at 9:59 PM (GMT 0) on 12 Nov 2019]
[edited by: Eugeny Brychkov at 9:59 PM (GMT 0) on 12 Nov 2019]
Parents Reply
  • Guenter, apologies - can you advise as a SME - if DCR of 5.5 Ohms (for part installed on this Altium board) or 7.7 Ohms (declared for B82422A1683K100) acceptable in this circuit, or should we strive for 130 mOhms (thus use big power inductor)?

    I am questioning so much about it because I have made proto board using AD725, and it appeared that Y-trap did more harm to the composite image than good. My belief that I have chosen wrong parts, or did wrong layout (it was made using P2P wiring - you can see the photo of it here, including the inductor I have chosen).

Children
  • The B82422.... should work fine.  5.5 vs 7.7 Ohm is not any real difference in the circuit.  

    Looking at the link for the board/schematic explains a lot.  Video and fly wires together make me cringe.  Never a good plan.

  • Guenter, great, thank you for the assessment (I have simulated it in LTspice to find out no much difference too). I agree with you, that was a quick proto showing that chip works, but I had a lot of problems during making it up and running more or less properly. I am working on the PCB implemeting experience gained and expecting it to have proper layout and performing well.

    I must say that image AD725 produces is superior - that's why I keep fighting having it in.

    Again thank you very much for your support.