About a specification of ADV7611

Hi,

I have a question of ADV7611.

I am reading the ADV7611 specification(Rev.D)

Page 12 has the following description.

------------------

PIXEL DATA OUTPUT MODES FEATURES
The output pixel port features include:
• 8-/12-bit ITU-R BT.656 4:2:2 YCrCb with embedded time codes and/or HS, VS, and FIELD output signals
• 16-/24-bit YCrCb with embedded time codes and/or HS and VS/FIELD pin timing
• 24-bit YCrCb/RGB with embedded time codes and/or HS and VS/FIELD pin timing
• DDR 8-/12-bit 4:2:2 YCrCb
• DDR 24-bit 4:4:4 RGB

------------------

I understand that "8-/12-bit ITU-R BT.656 4:2:2 YCrCb" can output VS and FIELD separately.

However, I am thinking about using it in "SDR4:2:2 16bit".

Q1)

In this case, can VS and FIELD not be output as separate signals?

Q2)

Which PIN is VS and FIELD output from?

Best regards,

Mountain999