Post Go back to editing

ADV7403

Thread Summary

The user is experiencing a blue screen output when configuring the ADV7403 for an analog RGB input from a PC at 1024x768 @ 60 Hz. The final answer suggests ensuring equal and minimized track lengths, using ferrite bead filters, and ground isolation for the RGB signals. The user confirms that CVBS inputs work, but the SSPD/STDI do not recognize the sync signals, despite good input signals and sync signals at the output.
AI Generated Content

Hello,

Regard ADV7403

Input Config:  Analog RGB form PC-Computer connected to ADV7403 on AIN1-Green AIN2 Blue AIN-3 Red Vsync to VS-IN, Hsync to HS_IN (All Other exactly as the EVB Schem)

Config Prime Mode 010b GR VID_STD 1100b for 1024x768 _@ 60 (Exactlly Out Put From My Computer Outputs)

Verfiy Input signal (Analog R,G,B ) and Vsyn,Hsync all signals O.K

Script Enter:

##CP XGA 1024x768##
:RGB  1024x768 _@ 60 ADV7402 65.000MHz Out through DAC:
42 05 02 ; Prim_Mode =010b for GR
42 06 0C ; VID_STD=1100b for 1024x768 _@ 60
42 1D 47 ; Enable 28MHz Crystal
42 3A 21 ; set latch clock settings to 010b, Power Down ADC3
42 3B 80 ; Enable External Bias
42 3C 5D ; PLL_QPUMP to 101b
42 6A 00 ; DLL Phase Adjust
42 6B C2 ; Swap Pr & Pb
42 73 90 ; Set man_gain
42 7B 1D ; TURN OFF EAV & SAV CODES Set BLANK_RGB_SEL
42 85 03 ; Enable DS_OUT
42 86 0B ; Enable stdi_line_count_mode
42 F4 3F ; Max Drive Strength
42 0E 80 ; ADI Recommended Setting
42 52 46 ; ADI Recommended Setting
42 54 00 ; ADI Recommended Setting
42 0E 00 ; ADI Recommended Setting
54 00 13 ; Power down Encoder
74 EE EE ; Power down HDMI
End

The output resualt is a Blue Screen !!! no meeter what we try to do the Outputs is a blue Screen

Register 0XB5[7] = 1 SSPD results not valid for read back

Register 0x86 [2] TRIG_STDI no trigger

No Valid data on BL[13:0] Block Length

Any suggest what we are doing worng !! Please advise

B.R

Moshe