ADV7411 primary mode and video standard settings in1600 x 900@60Hz

This is a question from my customer.
Please give advice from ADI engineers.
I'm using ADV7411 and assumption next input video format.
(1) 1920 x 1080p @ 60 Hz
(2) 1280 x 1024p @ 60 (SXGA)
(3) 1024 x 768p @ 60 (VGA)
(4) 1600 x 900 60p
In reference manual of ADV7611, next infomation is exist. Table 6. Primary Mode and Video Standard Selection
(1) PRIM_MODE[3:0] = 0101、VID_STD[5:0] = 011110(Input Video = HD 1x1、Output Resolution = 1920 x 1080)
(2) PRIM_MODE[3:0] = 0110、VID_STD[5:0] = 000101(Input Video = SXGA、Output Resolution = 1280 x 1024 @ 60)
(3) PRIM_MODE[3:0] = 0110、VID_STD[5:0] = 001100(Input Video = XGA、Output Resolution = 1024 x 768 @ 60)
I have question about primary mode and video standard settings, when input video format is (4).
Best regards
Parents
  • +1
    •  Analog Employees 
    on Aug 27, 2019 9:19 AM over 1 year ago

    Hi,

    PRIM_MODE and VID_STD are used to set up the free run modes.These controls are also used to specify the free run output standard.  You could not able to support the format which are not included in the video standard selection(VID_STD) table for free-run.

     But this format can be support by using any source equipment.

    Thanks,

    Poornima

Reply
  • +1
    •  Analog Employees 
    on Aug 27, 2019 9:19 AM over 1 year ago

    Hi,

    PRIM_MODE and VID_STD are used to set up the free run modes.These controls are also used to specify the free run output standard.  You could not able to support the format which are not included in the video standard selection(VID_STD) table for free-run.

     But this format can be support by using any source equipment.

    Thanks,

    Poornima

Children