Hell all,
When reserved pin No55, 57 and 59 are not used, are these pins open pin?
20 K ohm register is connected with Pin No 55 in datasheet P.22.
If No 55 is not used, is this pin left to open ?
Best Regards,
Daisu
AD8107
Production
The AD8106 and AD8107 are high speed, 16 × 5 video crosspoint
switch matrices. They offer a -3 dB signal bandwidth greater
than 260 MHz, and channel switch...
Datasheet
AD8107 on Analog.com
Hell all,
When reserved pin No55, 57 and 59 are not used, are these pins open pin?
20 K ohm register is connected with Pin No 55 in datasheet P.22.
If No 55 is not used, is this pin left to open ?
Best Regards,
Daisu