Hell all,
When reserved pin No55, 57 and 59 are not used, are these pins open pin?
20 K ohm register is connected with Pin No 55 in datasheet P.22.
If No 55 is not used, is this pin left to open ?
Best Regards,
Daisu
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
AD8107
Production
The AD8106 and AD8107 are high speed, 16 × 5 video crosspoint
switch matrices. They offer a −3 dB signal bandwidth greater
than 260 MHz, and channel...
Datasheet
AD8107 on Analog.com
Hell all,
When reserved pin No55, 57 and 59 are not used, are these pins open pin?
20 K ohm register is connected with Pin No 55 in datasheet P.22.
If No 55 is not used, is this pin left to open ?
Best Regards,
Daisu
Hello Daisu,
Pin 55 needs to be pulled up, as it is shown in the schematic, but pins 57 and 59 should be left open.
Best regards.
--Jonathan
Hello jpearson,
Thank you for your answer.
Can I ask one more question?
Please let me know why reserved pin 55 needs to be pull up with 20K ohm.
Best Regards,
Daisu
Hello Daisu,
Pin 55 is internally connected to a serial/parallel control, and must be pulled high to put the part in parallel mode. The part could work with serial control (that's what the other reserved pins are for), but a decision was made when the part was released to specify it for parallel-only operation.
Best regards,
--Jonathan
Hello jpearson,
Thank you for your answer.
Best Regards,
Daisu