Post Go back to editing

VGA to HDMI

I have to create a pcb module that has to do the following things: 

1) First of all take the VGA signal from a black box device (a device that exports vga signal Interlaced).

2) Then take the signal and make it digital and output it in HDMI in order to play in all random monitors.

My first idea was to use one of the following ICs to do the job : AD9983Α -> ADV7511 or ADV7520 and send the EDID commands via a microcontroller.

Is there an alternative way of doing it? And what commands i should send via EDID in order to display interlaced signal or it does deinterlacing in some way i don't understand.

Thanks in advance.

  • In general VGA is not interlaced.  Is the black box outputting 480i, 576i or maybe 720i?  The ADV7511 can handle all these formats

    Not all monitors and handle these formats.   Also the color space is important, 

    If there is any color space conversion or format conversion the the solution complexity went up a step.

    A microprocessor could handle the EDID transactions on the DDC bus but it would be much easier to just use a 24LCS22A EEPROM to store the EDID.

    Bottom line is I'd need to know exactly the output from the black box, format and color space to give a better recommendation 

  • Thanks a lot for the quick response the maximum resolution that the black box outputs does not exceed 720i, how can i check the color space conversion or format conversion in practice, because i don't have any information about it from the black box.

  • The only info that i found is that it uses this IC Bt481A in order to drive the VGA that IC supports multiple true-color modes and i think it uses the mode 8:8:8:8 so 24-bit with VGA overlay i don't know if that helps you enough.

    Thanks in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.