Post Go back to editing

Eval ADV8005 Analog Output scaling problem

Thread Summary

The user encountered issues with a 1024x768@60p DVI to 576i50 analog conversion using the EVAL ADV8005-8N, including a top bar and video cropping. The problem was resolved by using the SD encoder instead of the ED encoder, but RGB output was corrupted. The final solution suggested contacting sales support for further assistance with RGB output configuration.
AI Generated Content

Hi,

I am scaling a 1024x768@60p DVI video input to an analog 576@50i output (with EVAL ADV8005-8N).

command used:

-src HDMI 1

-mainvsp 576i50

-out comp 1 main

The conversion has the following two problems:

1) is present a bar on top of video that is not related to image (enlight in red in image)

2) the video is cut in all the direction (enlight in green in image)

do you know where can be the problem?

NOTE: I tried with two different monitor and the result was the same

Some update:

- we discovered that your script use the ED encoder even if the video is 576i50 (that is SD standard not ED). why you use ED encoder and not SD encoder? This can cause the problem that we are seeing on screen?

-we tried to use SD encoder and the conversion using SD encoder is good, no more cut or strange bar on top of video, but in SD mode we are able to go out only with YPbPr mode not in RGB. if we try to set RGB as output the signal is corrupted (no good signal avaiable on output).

below the setting we use:

i2c16w 1a e828 10
i2c16w 1a 1a04 22
i2c16w 1a 1a05 00
i2c16w 1a 1a06 04
i2c16w 1a 1a07 6c
i2c16w 1a 1b48 08
i2c16w 1a 1b30 87
i2c16w 1a 1b31 06
i2c16w 1a 1b32 19
i2c16w 1a 1b33 9e
i2c16w 1a 1b34 1f
i2c16w 1a 1b35 5d
i2c16w 1a 1b36 08
i2c16w 1a 1b37 00
i2c16w 1a 1b38 02
i2c16w 1a 1b39 ed
i2c16w 1a 1b3a 09
i2c16w 1a 1b3b d2
i2c16w 1a 1b3c 00
i2c16w 1a 1b3d fd
i2c16w 1a 1b3e 01
i2c16w 1a 1b3f 00
i2c16w 1a 1b40 1e
i2c16w 1a 1b41 63
i2c16w 1a 1b42 1a
i2c16w 1a 1b43 98
i2c16w 1a 1b44 07
i2c16w 1a 1b45 06
i2c16w 1a 1b46 08
i2c16w 1a 1b47 00
i2c16w 1a e881 ca
i2c16w 1a e884 00
i2c16w 1a e883 88
i2c16w 1a e882 11
i2c16w 1a e844 02
i2c16w 1a e845 C0
i2c16w 1a e846 02
i2c16w 1a e847 40
i2c16w 1a e84B 00
i2c16w 1a e849 10
i2c16w 1a e64b 11
i2c16w 1a e649 10
i2c16w 1a e401 00
i2c16w 1a e42a 25
i2c16w 1a e42b 34
i2c16w 1a e400 1E
i2c16w 1a e4e0 00
i2c16w 1a e402 10
i2c16w 1a e487 20
i2c16w 1a e828 11
i2c16w 1a e828 13
i2c16w 1a e828 17

The register that we use to set if RGB or YPbPr is e402 and we have the following behaviour:

i2c16w 1a e402 10 -> the RGB is set but no video on output

i2c16w 1a e402 20 -> the YPbPr is set, video on output OK

we tried also to put register e487 at 0xa0 ( so enable SD RGB input path) but with these enable on output we have only the synch whatever is the value of register e402.

Even with CSC enable on register F418 as suggest in another post the result is the same (no video output with RGB enable). 

regards,

Dario

Edit Notes

Update on TEST
[edited by: dn1993 at 8:59 AM (GMT 0) on 26 Jul 2019]
Parents Reply Children