[ADV7619] setting for "16bit SDR 422 Mode 0"

Hello,

Customer inquiry:

Do we have an exact configuration for "16 bit SDR 422 Mode 0"? I checkout out the "24 bit SDR 422 Mode 0" and modified only the register of 0x03 with my expected working mode, but it doesn't work.

Besides, this part of the whole configuration access always ends up with a failure.

72 01 00 ; Set N Value(6144)
72 02 18 ; Set N Value(6144)
72 03 00 ; Set N Value(6144)
72 15 01 ; Input 422 (YCrCb) with Separate Syncs, 44.1kHz fs
72 16 ED ; YCrCb 422 Style 3
72 18 46 ; CSC disabled
72 3B 80 ; PR Auto Mode
72 40 80 ; General Control Packet Enable
72 41 10 ; Power Down control
72 48 08 ; Data right justified
72 49 A8 ; Set Dither_mode - 12-to-10 bit
72 4C 04 ; 8 bit Output
72 55 20 ; Set YCrCb 422 in AVinfo Frame
72 56 08 ; Set active format Aspect
72 96 20 ; HPD Interrupt clear
72 98 03 ; ADI Required Write
72 99 02 ; ADI Required Write
72 9C 30 ; PLL Filter R1 Value
72 9D 61 ; Set clock divide
72 A2 A4 ; ADI Required Write
72 A3 A4 ; ADI Required Write
72 AF 16 ; Set HDMI Mode
72 BA 60 ; No clock delay
72 DE 9C ; ADI Required Write
72 E4 60 ; VCO Swing Reference Voltage
72 FA 7D ; Nbr of times to search for good phase

Best regards,

TH Kim