I2C register access configuration inquiry

Dear specialist,

I have checked out your forum link: https://ez.analog.com/video/w/documents/773/adv7619-design-support-files

My interested working scenario is 0x80 rather than your example of "98 03 82 ; 24 bit SDR 422 Mode 0", can I reuse this golden example by only overriding address 0x03 with the data of 0x80? If not, could you help to provide some working register configuration with the format of 0x80?

Another question about the indirect subaddress accessing, if you designate the the address which is not in Page 0, for example, "98 FB 68 ; HDMI". How should I assign the new subaddress? Is 0x68 a 8-bit address or 7-bit address? From my trial, it seems to me an 8-bit address.

Following your golden example of ":02-07 720p,1080i,1080p In - 24-bit YCbCr 422 Out:" I couldn't make these indirect accessing work, I got those errors for the last part of your configuration when I was trying to follow your example.

72 01 00 ; Set N Value(6144)
72 02 18 ; Set N Value(6144)
72 03 00 ; Set N Value(6144)
72 15 01 ; Input 422 (YCrCb) with Separate Syncs, 44.1kHz fs
72 16 ED ; YCrCb 422 Style 3
72 18 46 ; CSC disabled
72 3B 80 ; PR Auto Mode
72 40 80 ; General Control Packet Enable
72 41 10 ; Power Down control
72 48 08 ; Data right justified
72 49 A8 ; Set Dither_mode - 12-to-10 bit
72 4C 04 ; 8 bit Output
72 55 20 ; Set YCrCb 422 in AVinfo Frame
72 56 08 ; Set active format Aspect
72 96 20 ; HPD Interrupt clear
72 98 03 ; ADI Required Write
72 99 02 ; ADI Required Write
72 9C 30 ; PLL Filter R1 Value
72 9D 61 ; Set clock divide
72 A2 A4 ; ADI Required Write
72 A3 A4 ; ADI Required Write
72 AF 16 ; Set HDMI Mode
72 BA 60 ; No clock delay
72 DE 9C ; ADI Required Write
72 E4 60 ; VCO Swing Reference Voltage
72 FA 7D ; Nbr of times to search for good phase

Parents
  • 0
    •  Analog Employees 
    on Jul 16, 2019 1:32 PM

    The writes to address 72 are to a ADV7511 on another board.  If you are just dealing with the ADV7619 then you can ignore those writes.  These scripts are for a system with an ADV7619 and an ADV7511.

    Regarding 98 FB 68, the 68 is 8-bit addressing that the HDMI page will respond to.

    Changing 98 03 will change the output format as defined in the software manual.

Reply
  • 0
    •  Analog Employees 
    on Jul 16, 2019 1:32 PM

    The writes to address 72 are to a ADV7511 on another board.  If you are just dealing with the ADV7619 then you can ignore those writes.  These scripts are for a system with an ADV7619 and an ADV7511.

    Regarding 98 FB 68, the 68 is 8-bit addressing that the HDMI page will respond to.

    Changing 98 03 will change the output format as defined in the software manual.

Children