Post Go back to editing

Convert VGA input to CSI-2

Thread Summary

The user inquires about converting a 3-channel analog VGA input (1600x1200 @60fps) with HSYNC and VSYNC signals to MIPI CSI-2 for interfacing with an NVIDIA Jetson TX2 board. The final answer suggests using the ADV7401 to process the RGBHV signals and feeding its digital output to the ADV7482 for CSI-2 conversion. The ADV7482 does not support external HSYNC and VSYNC signals directly, but the combination of ADV7401 and ADV7482 can achieve the required conversion.
AI Generated Content

Does Analog Devices have any solution for a VGA input 1600x1200 @60fps and output is CSI-2 which is interfacing with nVIDIA jetson tx2 board.

Earlier I have seen the ADV7604 which has 1600x1200@60fps input and parallel output and after that i am using a bridge CMOS to CSI-2 but I am not sure about the parallel output of the ADV7604 which is DSI parallel or CSI-2 parallel .

 If there is any solution available from your side please let me know. 

Edit Notes

correction
[edited by: bankesh.roy at 4:35 AM (GMT 0) on 10 Jul 2019]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.