Post Go back to editing

Convert VGA input to CSI-2

Does Analog Devices have any solution for a VGA input 1600x1200 @60fps and output is CSI-2 which is interfacing with nVIDIA jetson tx2 board.

Earlier I have seen the ADV7604 which has 1600x1200@60fps input and parallel output and after that i am using a bridge CMOS to CSI-2 but I am not sure about the parallel output of the ADV7604 which is DSI parallel or CSI-2 parallel .

 If there is any solution available from your side please let me know. 



correction
[edited by: bankesh.roy at 4:35 AM (GMT 0) on 10 Jul 2019]
Parents Reply
  • Hi,

      Using AIN pins we can take the input from CVBS,Y/C ,YPrPb interface & generally it will decode the low formats like PAL,NTSC,SECAM etc.

    However HDMI capable receiver supports a maximum pixel clock frequency of 162 MHz, allowing HDTV formats up to 1080p, and display resolutions up to UXGA (1600 × 1200 at 60 Hz).

    But we haven't try the VGA input using AIN pins with this ADV7482 part, Please try with VGA input using AIN pins & let us know.

    Thanks,

    Poornima

Children