graphics modes with ADV7341

I want to use graphics modes (vga, xga, sxga, wxga, etc) with the 7341. I see the question was answered, but NO LINKS WERE GIVEN TO THE ANSWERS! One would think this would be information useful to many, so why is it not readily available? Are there registers setting for these modes? Can the 7341 be configured to slave itself to any input timing, assuming either the external syncs or embedded timing is used?