Post Go back to editing

ADV7842 I2S output with compressed audio input

Thread Summary

The user encountered issues with no I2S output on AP1 when receiving Dolby Digital audio over HDMI with the ADV7842. The solution involved setting bit 7 of the HDMI Map 0x03 register (DIS_I2S_ZERO_COMPR) to 1, which is not documented in the current HW reference manual. The engineer provided the documentation for this bit and a related one (NEW_MUTE_COMPRS) that will be included in the next revision of the docs.
AI Generated Content

This is an open letter to the ADV7842 design team.

I was not able to get any output on AP1 in the I2S format with a compressed audio signal (Dolby Digital) coming in over HDMI. Every status indicator showed that it should be working and that audio was unmuted. I tried playing with I2SOUTMODE and finally found some activity on the pin when I set it to RAW SPDIF. But the SPDIF signal didn't look right so I set it back to I2S mode and just for the heck of it I tried setting bit 7 of the register (HDMI Map 0x03). Lo and behold I got the correct I2S output!

Bit 7 in this register is not documented in the HW reference manual or the register map. This register is not written to in any of the HDMI scripts. Needless to say I am really pissed off about the lack of documentation, having wasted several days trying to get it to work. This is such a basic operation for this part, most cable channels use Dolby Digital for their audio, that I can't believe this wouldn't have been tested and documented properly.

  • Hello,

    Sorry for your frustration, we've gone through it even with our own evaluation boards at times! Getting all the hidden bits documented is a constant fight between what is needed and what will cause more problems.  We've been making some progress, but it's never as easy and fast as it should be.

    I'll make sure your input gets seen.

    Dave

  • Hello,

    Too late I know but for what it's worth... I got the documentation for that bit and a related one and they'll be in the next revision of the docs:

    NEW_MUTE_COMPRS (HDMI, 0x1A [7])

    Configures the audio mute function

    • 0 = The part mutes the audio data it outputs in I2S format if it receives compressed audio and the mute mask MT_MSK_COMPRS_AUD is set high. The mute circuit mutes the audio data by ramping down the outgoing audio data.

    • 1 [Default] = See the description of DIS_I2S_ZERO_COMPR.

    DIS_I2S_ZERO_COMPR (HDMI 0x3 [7])

    Enable/Disable zero’ing of I2S data. This control is effective when NEW_MUTE_COMPRS is set high.

    • 0[Default]  = The reception of compressed audio does not cause the part to mute the I2S output (i.e. MT_MSK_COMPRS_AUD has no effect) but rather to zero audio data output via the I2S outputs. If any other mute condition causes a mute while compressed audio is received (e.g. loss of TMDS clock) all output are not ramped down but rather zero’ed sharply.

    • 1 = The reception of compressed audio does not cause the part to mute the I2S output (i.e. MT_MSK_COMPRS_AUD has no effect) nor to zero audio data output via the I2S outputs. If any other mute condition causes a mute while compressed audio is received (e.g. loss of TMDS clock) all output are not ramped down but rather zero’ed sharply

    Dave