ADV7619 I2S Audio Stream AP pin assignments

Hello Specialist,

I am implementing the schematic design for the ADV7619 part, I am very confused about the pin assignments when it is configured as I2S mode. Please help to clarify here.

  1. In your latest revision D datasheet, in the pin description on Page 12, you don't mention AP1 can be configured as I2S data. On the other hand, In Figure 5 I2S Timing, you specify the I2Sx data are distributed from AP1 to AP4. Is it a contradictory here, which one should I follow?
  2. After answering the first question, what is the first data channel? Is the audio data distributed sequentially from AP1 to AP4?
  3. I am really confused about your I2S timing diagram, it is quite different with the command standard I2S format, typically, a I2S needs a word clock.and a bit clock, are the LRCLK and SCLK in your diagram just the word clock.and bit clock respectively?
  4. Some audio chip needs to be fed a master clock, does ADV7619 need a master clock when working as the I2S mode? your Figure 5 timing diagram doesn't mention that at all. In your pin description, MCLK is an output rather than an input.
  5. What is the functionality of AP0, if I only need to support I2S, I don't need it at all, is that correct?
  6. Are the I2S modes of LEFT-JUSTIFIED and RIGHT-JUSTIFIED completely configured by I2C registers rather than physical pins?

Looking forward to your reply. Thanks.

Top Replies

Parents
  • 0
    •  Analog Employees 
    on May 6, 2019 11:13 AM over 1 year ago

    Hi,

     1) In your latest revision D datasheet, in the pin description on Page 12, you don't mention AP1 can be configured as I2S data. On the other hand, In Figure 5 I2S Timing, you specify the I2Sx data are distributed from AP1 to AP4. Is it a contradictory here, which one should I follow?  

      As per expert comment, AP1...AP4 are the only pins that can output I2S signals.

      For Page 10, Table 5, AP0, the description looks like a copy/paste typo.

    2) After answering the first question, what is the first data channel? Is the audio data distributed sequentially from AP1 to AP4?

        Yes.

    3) I am really confused about your I2S timing diagram, it is quite different with the command standard I2S format, typically, a I2S needs a word clock.and a bit clock, are the LRCLK and SCLK in your diagram just the word clock.and bit clock respectively?

     Yes,Please refer here en.wikipedia.org/.../I²S

    Note: 1.Bit clock line
    Officially "continuous serial clock (SCK)".[1] Typically written "bit clock (BCLK)".

    2.Word clock line
     Officially "word select (WS)".Typically called "left-right clock (LRCLK)" or "frame sync (FS)".
     0 = Left channel, 1 = Right channel

    4) Some audio chip needs to be fed a master clock, does ADV7619 need a master clock when working as the I2S mode? your Figure 5 timing diagram doesn't mention that at all. In your pin description, MCLK is an output rather than an input.

       Yes, ADV7619 has TMDS input,from that TMDS,audio DPLL is used to generate the internal audio master clock with a frequency of 128 times the audio sampling frequency, usually called fs.The audio master clock is used to clock the audio processing section.
      The ADV7619 also regenerates an audio master clock along with the extraction of the audio data.The clock regeneration is performed by an integrated DPLL.

    5) Are the I2S modes of LEFT-JUSTIFIED and RIGHT-JUSTIFIED completely configured by I2C registers rather than physical pins?

          Yes.

    Thanks,

    Poornima

  • Hello Poornima,

    Thanks for your quick response, and most questions are well answered. 

    I have only one question left about the MCLK. In I2S mode, it is an output rather than input. do we need to feed it with a frequency of 128fs? If yes, how should we generate this clock?

  • 0
    •  Analog Employees 
    on May 6, 2019 1:10 PM over 1 year ago in reply to CYun396

    Hi,

     MCLK is derived from the TMDS clock and the information in the audio infoframe. For more details please refer Audio and control configuration section in ADV7619 Reference Manual.

     

    And also the frequency of audio master clock MCLKOUT is set using the MCLK_FS_N[2:0] register,it can selects the frequency of MCLK out as multiple of 128fs.

    Thanks,

    Poornima

  • Thanks Poornima, as far as I understand from your enlightenment, if I only need to support 4 channels of audio data under I2S mode, the minimum IO number I need is 6, the pins needed are AP1~AP5 and SCLK. AP0 is not involved, and MCLK is not mandatory provided that I can latch the data by using SCLK and LRCLK only. Is that right?

Reply Children