Post Go back to editing

ADV7513 Max Transmitter Total Power

Hi,

ADV7513 Hardware User's Guide Rev. 0 Page 40 describes 'In Section 4: the specifications table lists the maximum power as 326mW

at 1080p, CSC off.'

But Section 4 describes that Max Transmitter Total Power equals 256mW.

On the other hand ADV7511 Max Transmitter Total Power seems to be equal to 326mW according to ADV7511 Data sheet.

Is '326mW' described ADV7513 Hardware User's Guide Rev. 0 Page 40 typo?

Thanks.

Parents
  • Hi,

      You are correct, the max power for the ADV7513 is 256mW. The value on page 40 of the Hardware User's Guide was from the ADV7511. Because the ADV7513 is only running 24 bits of data as well as a few other minor differences from the ADV7511, the maximum power consumption can be brought down from the 326mW value.

         I will begin a revision of the ADV7513 Hardware User's Guide - thanks for bringing this to our attention.

    Best,

    Chris

Reply
  • Hi,

      You are correct, the max power for the ADV7513 is 256mW. The value on page 40 of the Hardware User's Guide was from the ADV7511. Because the ADV7513 is only running 24 bits of data as well as a few other minor differences from the ADV7511, the maximum power consumption can be brought down from the 326mW value.

         I will begin a revision of the ADV7513 Hardware User's Guide - thanks for bringing this to our attention.

    Best,

    Chris

Children
No Data