Post Go back to editing

ADV7511W and ADV7511 (non-W) register compatible with ADV7513 ?

Thread Summary

The user inquired about the register compatibility between ADV7511 and ADV7513/ADV7511W. The support engineer confirmed that the register differences are minor, making it possible to develop code on the Xilinx board with ADV7511 and migrate it to an ADV7513/ADV7511W design seamlessly, provided no ADV7511-specific features are used.
AI Generated Content

Hello,

My understanding is that the ADV7511W Tx is identical to ADV7513 (http://www.analog.com/en/audiovideo-products/analoghdmidvi-interfaces/adv7513/products/product.html) Tx in form, fit, and function (pins for pin, same software / register identical).

Essentially, the two can be used interchangeably, as the register configuration is the same.

I have a customer that found a Xilinx reference design that is using an ADV7511 (different pinout than "W") and is asking if that version of the part is also register compatible with the ADV7513. Ideally, they want to develop the code on the Xilinx board and move it over to their ADV7513/ADV7511W design seamlessly.

Let me know if you think this is possible.

Mike