Hallo,
i want to use the AD8195 like shown in figure 4 or figure 34 in the current datasheet (hdmi source > 20m cable > EDID-EEPROM / AD8195 > HDMI Sink).
This means all signals (HDMI and DDC) are much longer then they should be normally.
* HDMI signals will be boosted from the AD8195 -> all fine!
* DDC signals are not boosted by the AD8195 -> all fine?
An this leads to my question:
If i use the maximal length of a hdmi cable mentioned in the datasheet (= 20 m) could the hdmi-source read the edid-eeprom correctly if its placed like shown in figure 34 (typical edid placement - before the AD8195)?
Best Regards Eric